Sleep mode current increases when i2c wakeup source used

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sleep mode current increases when i2c wakeup source used

1,965件の閲覧回数
VasuVirpariya
Contributor II

I used the SDK's example (power_mode_switch_lpc) for exercising power-down mode. I added support for i2c wakeup in power-down mode. The issue that we are facing is as per below.

1) Entering power-down mode from the UART menu.

2) Power down mode current = 14 uA.

3) Wake up from the I2C.

4) Entering power-down mode from the UART menu.

5) Power down mode current = 67 uA.

 I have attached the project below. What could be going wrong in second time?

 

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,946件の閲覧回数
VasuVirpariya
Contributor II

It is LPC804. I am using the LPCxpresso804 kit. 

What I am wondering is why first time it is consuming 14uA current and the second time onward it is taking 67uA. The attached firmware can be run on the LPCxpresso804 kit.

0 件の賞賛
返信

1,950件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Because you use I2C as slave to wake-up the LPC, I suppose that you activate  SRAM block, as you know that each SRAM block requires a lot power.

Pls check the SRAM block power up or down in PDRUNCFG register for your different configuration

BTW, can you tell us the part number of LPC?

BR

XiangJun Rong

0 件の賞賛
返信