Single Wire Debugging (SWD) with 1 MHz System Clock does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Wire Debugging (SWD) with 1 MHz System Clock does not work

3,789 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Mon Feb 17 08:32:18 MST 2014
Clock Setup: Clock source is the internal IRC.

When I leave the divider by 1, then SWD still works.

When I change the divider to 12 (eq. 1 MHz) then it get "Failed on connect: Ep(01). Target marked as not debuggable"

What's wrong?
Labels (1)
0 Kudos
Reply
5 Replies

3,750 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 04:01:54 MST 2014
Thanks, I changed the debug speed and it is fixed.
0 Kudos
Reply

3,750 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 03:32:18 MST 2014

Quote: starblue
Try lowering the SWD clock frequency.



How?
0 Kudos
Reply

3,750 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 03:31:55 MST 2014
It's an LPC812 and a Red Probe+
0 Kudos
Reply

3,750 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Mon Feb 17 10:01:28 MST 2014
Try lowering the SWD clock frequency.
0 Kudos
Reply

3,750 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 17 09:03:50 MST 2014
Which target?
Which debug probe?
0 Kudos
Reply