Single Wire Debugging (SWD) with 1 MHz System Clock does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Single Wire Debugging (SWD) with 1 MHz System Clock does not work

3,747件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Mon Feb 17 08:32:18 MST 2014
Clock Setup: Clock source is the internal IRC.

When I leave the divider by 1, then SWD still works.

When I change the divider to 12 (eq. 1 MHz) then it get "Failed on connect: Ep(01). Target marked as not debuggable"

What's wrong?
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,708件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 04:01:54 MST 2014
Thanks, I changed the debug speed and it is fixed.
0 件の賞賛
返信

3,708件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 03:32:18 MST 2014

Quote: starblue
Try lowering the SWD clock frequency.



How?
0 件の賞賛
返信

3,708件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pkarrer_solcept on Wed Feb 19 03:31:55 MST 2014
It's an LPC812 and a Red Probe+
0 件の賞賛
返信

3,708件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Mon Feb 17 10:01:28 MST 2014
Try lowering the SWD clock frequency.
0 件の賞賛
返信

3,708件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 17 09:03:50 MST 2014
Which target?
Which debug probe?
0 件の賞賛
返信