Simple pin function name quesiton

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Simple pin function name quesiton

1,730 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Dec 18 09:29:10 MST 2014
In UM10430 there are pin functions: USB0_PPWR and USB0_PWR_EN.

Are these the same signal?

Thanks
标签 (1)
0 项奖励
回复
2 回复数

1,706 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Fri Dec 19 06:36:41 MST 2014
Thanks.

Trying not to be a pest...
This is only my 1st pass through the doco and I am just trying to make sure all my peripherals will work with the pinmux.

Then I discovered the pinmux tool.  Very well done tool and and saved me hours.

Tony
0 项奖励
回复

1,706 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Thu Dec 18 11:18:55 MST 2014
Hi tvink,

I can see the source of confusion because the two different pin mutiplexing table do not correlate. Yes, the two pin functions have the same role. I believe the reason for the different names is simply due to UM upkeep. I'll report it to the tech writers so it will be fixed in the next revision. :)

Thank you.
0 项奖励
回复