Simple pin function name quesiton

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple pin function name quesiton

1,764 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Dec 18 09:29:10 MST 2014
In UM10430 there are pin functions: USB0_PPWR and USB0_PWR_EN.

Are these the same signal?

Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Fri Dec 19 06:36:41 MST 2014
Thanks.

Trying not to be a pest...
This is only my 1st pass through the doco and I am just trying to make sure all my peripherals will work with the pinmux.

Then I discovered the pinmux tool.  Very well done tool and and saved me hours.

Tony
0 Kudos
Reply

1,740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Thu Dec 18 11:18:55 MST 2014
Hi tvink,

I can see the source of confusion because the two different pin mutiplexing table do not correlate. Yes, the two pin functions have the same role. I believe the reason for the different names is simply due to UM upkeep. I'll report it to the tech writers so it will be fixed in the next revision. :)

Thank you.
0 Kudos
Reply