Signature LPC17xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Signature LPC17xx

1,406件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mauricio1976 on Fri Oct 23 10:19:12 MST 2015
Hello,
I am working on a project with bootloader. I used LPC1769 and LPCXpresso v7.9.2 [Build 493] [2015-09-14]. The application that will be load in the flash memory must be validated. Thus i think generate a signature for the aplication file and after charge the application recalculate the signature and compare with the original.
I read the document "AN10918 NXP LPC Cortex-M3 IEC60335 Class B library" and i use the functions:
void StartHardSignatureGen (uint32_t startAddr, uint32_t length, FlashSign_t *pResultSign)
void StartSoftSignatureGen (uint32_t startAddr, uint32_t length, FlashSign_t *pResultSign)

The signature generated for each one of this functions must be the same, but i have an error and i don't know where.

The function "StartSoftSignatureGen" in the "AN10918" it is the same that the algorithm "Fig 140. Algorithm for generating a 128 bit signature" in pag. 650 in document "UM10360"?
There are some example with IEC60335 (Flash) for LPCXpresso?

Thanks, Mauricio
ラベル(1)
0 件の賞賛
返信
1 返信

1,342件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mauricio1976 on Tue Nov 03 13:55:27 MST 2015
Hello, somebody could help me?
Thanks, Mauricio

Quote: mauricio1976
Hello,
I am working on a project with bootloader. I used LPC1769 and LPCXpresso v7.9.2 [Build 493] [2015-09-14]. The application that will be load in the flash memory must be validated. Thus i think generate a signature for the aplication file and after charge the application recalculate the signature and compare with the original.
I read the document "AN10918 NXP LPC Cortex-M3 IEC60335 Class B library" and i use the functions:
void StartHardSignatureGen (uint32_t startAddr, uint32_t length, FlashSign_t *pResultSign)
void StartSoftSignatureGen (uint32_t startAddr, uint32_t length, FlashSign_t *pResultSign)

The signature generated for each one of this functions must be the same, but i have an error and i don't know where.

The function "StartSoftSignatureGen" in the "AN10918" it is the same that the algorithm "Fig 140. Algorithm for generating a 128 bit signature" in pag. 650 in document "UM10360"?
There are some example with IEC60335 (Flash) for LPCXpresso?

Thanks, Mauricio


0 件の賞賛
返信