Setting up LPCXpresso v8.2.2 in Ubuntu 16.10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up LPCXpresso v8.2.2 in Ubuntu 16.10

1,431 Views
johnygeorgemala
Contributor I

I am trying to install the LPCXpresso v8.2.2  in Ubuntu 16.10. I did everything and installed the stuffs as per the readme given.

Now I am trying to connect to a LPC824 Max board. Ubuntu detects the board. I am trying to debug a sample application and I have the following error.

LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:13:28 - crt_emu_cm_redlink build 725)
Failed on connect: Ee(36). Could not connect to core.
No connection to emulator device

How to fix it ?

0 Kudos
Reply
1 Reply

1,266 Views
converse
Senior Contributor V
0 Kudos
Reply