Setting up 2 USARTs with DMA for LPC54018J4MET180, USART9 does not receive any data via DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Setting up 2 USARTs with DMA for LPC54018J4MET180, USART9 does not receive any data via DMA

跳至解决方案
1,613 次查看
jchen2023
Contributor II

We plan to use 2 usarts from LPC54018J4MET180, USART2 and USART9 on two different baud rates, one faster and the other slower. Our experience so far is that both of them can send with the configured baud rates but only one receives data via DMA0 on channel 4 and the other one does not receive anything on channel 22.

We want to get expert advice on the feasibility and the correct configurations step for both of them work the same time.

We are using Keil compiler and Arm\Packs\NXP\LPC54018M_DFP\12.2.1.

标签 (1)
0 项奖励
回复
1 解答
1,559 次查看
jchen2023
Contributor II

Found an issue with the data receive code, it failed to call USART_TransferReceiveDMA for USART9. That's the reason, there is not data received via DMA. The above initUsart code works.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,560 次查看
jchen2023
Contributor II

Found an issue with the data receive code, it failed to call USART_TransferReceiveDMA for USART9. That's the reason, there is not data received via DMA. The above initUsart code works.

0 项奖励
回复
1,560 次查看
jchen2023
Contributor II

Found issues in my receive code that checks the buffer size. It didn't call the USART_TransferReceiveDMA for USART9. The above usartInit code works. Please close this out as solved.

0 项奖励
回复
1,603 次查看
jchen2023
Contributor II

Here is the uart set up code that results in USART2 working but USART9 doesn't receive from DMA:

/*****************************************************************************

* Local types and defines

*****************************************************************************/

 

#define RX_DMA_CHANNEL_FLEXCOMM2_RX 4

#define RX_DMA_CHANNEL_FLEXCOMM9_RX 22

 

/*****************************************************************************

* Local variables

*****************************************************************************/

 

static usart_dma_handle_t dmaHandle = {0};

 

static dma_handle_t rxHandle = {0};

 

static char printBuf[256] = {0};

 

static const char *CRLF = "\r\n";

 

 

static usart_dma_handle_t dmaHandle_0 = {0};

 

static dma_handle_t rxHandle_0 = {0};

 

static bool uart_status2 = false;  

static bool uart_status9 = false;

 

/*****************************************************************************

* Public functions

*****************************************************************************/

 

/**

* \brief Initialize the USART interface.

*/

void initUsart(void)

{

 

 

 

   // Connectivity port -

   CLOCK_AttachClk(kFRO12M_to_FLEXCOMM9);

   RESET_PeripheralReset(kFC9_RST_SHIFT_RSTn);

 

 

   DMA_Init(DMA0);

 

   usart_config_t config2 = {0};

   USART_GetDefaultConfig(&config2);

   config2.baudRate_Bps = 115200;

   config2.enableTx = true;

   config2.enableRx = true;

 

   USART_Init(USART9, &config2, CLOCK_GetFlexCommClkFreq(9));

 

   DMA_EnableChannel(DMA0, RX_DMA_CHANNEL_FLEXCOMM9_RX);

   DMA_CreateHandle(&rxHandle_0, DMA0, RX_DMA_CHANNEL_FLEXCOMM9_RX);

 

   if (kStatus_Success != USART_TransferCreateHandleDMA(USART9, &dmaHandle_0, NULL, NULL, NULL, &rxHandle_0))

   {

      uart_status9 = true;

   }

      

   CLOCK_AttachClk(kFRO12M_to_FLEXCOMM2);

   RESET_PeripheralReset(kFC2_RST_SHIFT_RSTn);

 

   usart_config_t config = {0};

   USART_GetDefaultConfig(&config);

   config.baudRate_Bps = 750000;

   config.enableTx = true;

   config.enableRx = true;

 

   USART_Init(USART2, &config, CLOCK_GetFlexCommClkFreq(2));

 

   DMA_EnableChannel(DMA0, RX_DMA_CHANNEL_FLEXCOMM2_RX);

   DMA_CreateHandle(&rxHandle, DMA0, RX_DMA_CHANNEL_FLEXCOMM2_RX);

 

   if (kStatus_Success == USART_TransferCreateHandleDMA(USART2, &dmaHandle, NULL, NULL, NULL, &rxHandle))

   {

      uart_status2 = true;

 

   }

 

 

}

0 项奖励
回复