Serial Communications with MBED LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial Communications with MBED LPC1768

2,551 次查看
AndrewJKnowles
Contributor I

Hi,

I am currently using the MBED LPC1768 Microcontroller in a project where I wish to communicate with either MBED studio or a terminal emulator such as CoolTerm however, the device does not communicate at all. At first I though it maybe a programming issue so I tried the same code on a NUCLEO-L476RG and It worked perfectly, both within MBED Studio and in CoolTerm. The code its self quite simply prints "hello" using printf inside an infinite while loop.

Additionally, windows intermittently does not recognise the device however, it does still appear as a storage device and I am still able to run programs that do not utilise printf or make use of the serial libraries found in MBED OS.

I just wondered if there is a solution to this issue?

 

Note:

firmware version: 141212

MBED OS: 6.16

 

many thanks,

Andrew

标签 (2)
0 项奖励
回复
1 回复

2,534 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @AndrewJKnowles ,

About the MBED, recommend you ask help from MBED website: https://forums.mbed.com/categories  

there are MBED experts know MBED issue well. 

 

BR

Alice

 

 

0 项奖励
回复