Sending bulk data over USB using CDC ROM Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sending bulk data over USB using CDC ROM Drivers

2,089 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sarangkalbande on Thu Sep 12 23:12:21 MST 2013
Hi,
I am working on LPC 11U37 USB ROM Project.
I have keil CDC example(UART USB Bridge) which is working fine.
whenever I write something on UART Serial terminal,I get it on USB virtual terminal and
Vice versa.

But when I try to implement some logic inside while(1) loop like sending buffer of 16 bytes
It always fails.I think the problem with sequencing.

Can anyone tell me how to send buffer data using USB CDC?kindly provide example or the steps I need to follow
to achieve the same?
Labels (1)
0 Kudos
Reply
2 Replies

1,987 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sarangkalbande on Tue Sep 17 02:45:17 MST 2013
Hi,
Thanks for the reply
Please find the code below

int main (void)
{
  USBD_API_INIT_PARAM_T usb_param;
  USBD_CDC_INIT_PARAM_T cdc_param;
  USB_CORE_DESCS_T desc;
  USBD_HANDLE_T hUsb, hCdc;
  ErrorCode_t ret = LPC_OK;
  uint32_t ep_indx;

  nfcInProgress = 0;

#ifdef UART
    UART_Init(9600);

    //Priority = 1;
    //IsDataAvailable = 1;
   #else
    RS485_Init(BaudRate);
   #endif
Timer_Init();
TimerOut=Timer_New(TIMEMS);
BuzzerTimer=Timer_New(TIMEMS);
Gpio_Init();
Buzzer_Init();
Relay_Init();
UART_BuffFlush();
Flush_SendDataBuff();
Flush_CardDataBuff();

phpalI14443p3a_Sw_DataParams_t I14443p3a;
phpalI14443p4_Sw_DataParams_t I14443p4;
   phpalMifare_Sw_DataParams_t palMifare;
   phKeyStore_Rc663_DataParams_t Rc663keyStore;
phbalReg_Stub_DataParams_t balReader;
   phhalHw_Rc663_DataParams_t halReader;
phalMfc_Sw_DataParams_t alMfc;
phStatus_t status;
uint8_t bUid[10];
uint8_t bLength;
uint8_t bMoreCardsAvailable;
uint8_t bSak[1];
uint8_t bHalBufferReader[0x40];
Reset_RC663();
   phbalReg_Stub_Init(&balReader, sizeof(phbalReg_Stub_DataParams_t));

   PH_CHECK_SUCCESS_FCT(status,phhalHw_Rc663_Init(&halReader,sizeof(phhalHw_Rc663_DataParams_t),
            &balReader, 0, bHalBufferReader, sizeof(bHalBufferReader),
            bHalBufferReader, sizeof(bHalBufferReader)));

   halReader.bBalConnectionType = PHHAL_HW_BAL_CONNECTION_SPI;
   pHal = &halReader;
   PH_CHECK_SUCCESS_FCT(status, phpalI14443p3a_Sw_Init(&I14443p3a,
                        sizeof(phpalI14443p3a_Sw_DataParams_t), pHal));

   PH_CHECK_SUCCESS_FCT(status,phpalI14443p4_Sw_Init(&I14443p4,
                sizeof(phpalI14443p4_Sw_DataParams_t), pHal));

   PH_CHECK_SUCCESS_FCT(status,phpalMifare_Sw_Init(&palMifare,
                sizeof(phpalMifare_Sw_DataParams_t), pHal, &I14443p4));

   PH_CHECK_SUCCESS_FCT(status,phKeyStore_Rc663_Init(&Rc663keyStore,
                sizeof(phKeyStore_Rc663_DataParams_t), pHal));

   PH_CHECK_SUCCESS_FCT(status,phalMfc_Sw_Init(&alMfc,
                sizeof(phalMfc_Sw_DataParams_t), &palMifare, NULL));

   PH_CHECK_SUCCESS_FCT(status,phhalHw_FieldReset(pHal));

   PH_CHECK_SUCCESS_FCT(status,phhalHw_ApplyProtocolSettings(pHal,
                PHHAL_HW_CARDTYPE_ISO14443A));


   #ifdef RS485
       RS485_ReceiveEnable();
   #endif

   Buzzer_SetState(BUZ_OFF);




  volatile uint32_t s,p;
//volatile uint32_t i;
  LPC_SYSCON->SYSAHBCLKCTRL |= (1<<6);
  /* Port PIO0_17 is used for Buzzer control*/
  LPC_IOCON->PIO0_17 |= 0x00;
  LPC_GPIO->DIR[0] |= (1<<17);

  SystemCoreClockUpdate ();

  /* get USB API table pointer */
  pUsbApi = (USBD_API_T*)((*(ROM **)(0x1FFF1FF8))->pUSBD);

  /* enable clocks and pinmux for usb0 */
  USB_pin_clk_init();

  /* initilize call back structures */
  memset((void*)&usb_param, 0, sizeof(USBD_API_INIT_PARAM_T));
  usb_param.usb_reg_base = LPC_USB_BASE;
  usb_param.mem_base = 0x10001000;
  usb_param.mem_size = 0x1000;
  usb_param.max_num_ep = 3;

  /* init CDC params */
  memset((void*)&cdc_param, 0, sizeof(USBD_CDC_INIT_PARAM_T));
  memset((void*)&g_vCOM, 0, sizeof(VCOM_DATA_T));

  /* user defined functions */
#if defined(UART_BRIDGE)
  cdc_param.SetLineCode = VCOM_SetLineCode;
  usb_param.USB_SOF_Event = VCOM_sof_event;
#endif
  cdc_param.SendBreak = VCOM_SendBreak;

  /* Initialize Descriptor pointers */
  memset((void*)&desc, 0, sizeof(USB_CORE_DESCS_T));
  desc.device_desc = (uint8_t *)&VCOM_DeviceDescriptor[0];
  desc.string_desc = (uint8_t *)&VCOM_StringDescriptor[0];
  desc.full_speed_desc = (uint8_t *)&VCOM_ConfigDescriptor[0];
  desc.high_speed_desc = (uint8_t *)&VCOM_ConfigDescriptor[0];

  /* USB Initialization */
  ret = pUsbApi->hw->Init(&hUsb, &desc, &usb_param); 
  if (ret == LPC_OK) {

    // init CDC params
    cdc_param.mem_base = usb_param.mem_base;
    cdc_param.mem_size = usb_param.mem_size;
    cdc_param.cif_intf_desc = (uint8_t *)&VCOM_ConfigDescriptor[USB_CONFIGUARTION_DESC_SIZE];
    cdc_param.dif_intf_desc = (uint8_t *)&VCOM_ConfigDescriptor[USB_CONFIGUARTION_DESC_SIZE + \
                               USB_INTERFACE_DESC_SIZE + 0x0013 + USB_ENDPOINT_DESC_SIZE ];

    ret = pUsbApi->cdc->init(hUsb, &cdc_param, &hCdc);

    if (ret == LPC_OK) {
      /* store USB handle */
      g_vCOM.hUsb = hUsb;
      g_vCOM.hCdc = hCdc;
      g_vCOM.send_fn = VCOM_usb_send;

      /* allocate transfer buffers */
      g_vCOM.rxBuf = (uint8_t*)(cdc_param.mem_base + (0 * USB_HS_MAX_BULK_PACKET));
      g_vCOM.txBuf = (uint8_t*)(cdc_param.mem_base + (1 * USB_HS_MAX_BULK_PACKET));
      cdc_param.mem_size -= (4 * USB_HS_MAX_BULK_PACKET);

      /* register endpoint interrupt handler */
      ep_indx = (((USB_CDC_EP_BULK_IN & 0x0F) << 1) + 1);
      ret = pUsbApi->core->RegisterEpHandler (hUsb, ep_indx, VCOM_bulk_in_hdlr, &g_vCOM);
      if (ret == LPC_OK) {
        /* register endpoint interrupt handler */
        ep_indx = ((USB_CDC_EP_BULK_OUT & 0x0F) << 1);
        ret = pUsbApi->core->RegisterEpHandler (hUsb, ep_indx, VCOM_bulk_out_hdlr, &g_vCOM);
        if (ret == LPC_OK) {
         
          /* enable IRQ */
          NVIC_EnableIRQ(USB_IRQn); //  enable USB0 interrrupts

       //   pUsbApi->hw->WriteEP(hUsb,USB_CDC_EP_BULK_IN,
                      // &buff[0], 5);


#if defined(UART_BRIDGE)
          g_vCOM.send_fn = VCOM_uart_send;

         // g_vCOM.send_fn = pUsbApi->hw->WriteEP(hUsb,USB_CDC_EP_BULK_IN,&buff[0], 5);
          /* init UART for bridge */
          init_uart1_bridge(&g_vCOM, 0);
          /* enable IRQ */
          NVIC_EnableIRQ(UART_IRQn); //  enable Uart interrrupt
#endif
          /* USB Connect */
         pUsbApi->hw->Connect(hUsb, 1);
       /*   LPC_GPIO->SET[0] = (1<<17);
          for(p=0;p<25;p++)
          {
          for(s=0xfffff;s>0;s--);

          }
          LPC_GPIO->CLR[0] = (1<<17);*/
        // pUsbApi->hw->WriteEP(hUsb,USB_CDC_EP_BULK_IN,
                              // &buff[0], 5);


        }
      }
    }   
  }
  /* wait for ever in uart bridge mode */
while (1)
  {
if (IsDataAvailable==0)
   {



//nfcInProgress = 1;
    status=phpalI14443p3a_ActivateCard(&I14443p3a, NULL, 0x00, bUid, &bLength,
                                              bSak, &bMoreCardsAvailable);

     if (status != PH_ERR_SUCCESS)
        {
     Buzzer_Off();
     IsDataAvailable=0;

        }
     else
        {


     status = phalMfc_Authenticate(&alMfc, BLOCK_AUTHENTICATE, PHHAL_HW_MFC_KEYA,
                                         0, 0, bUid, bLength);
     //UART_SendChar(status);
     //nfcInProgress = 0;

      if (status != PH_ERR_SUCCESS)
                {

             Buzzer_Fail();
             IsDataAvailable=0;

                }
              else
                 {
                   status = phalMfc_Read(&alMfc, 2, &CardDataBuffer[0]);
                   if (status != PH_ERR_SUCCESS)
                     {

                       Buzzer_Fail();
                       IsDataAvailable=0;


                      }
                   else
                      {
                   Buzzer_Pass();

                  // UART_Send(&CardDataBuffer[0],0x10);


                   pUsbApi->hw->WriteEP(hUsb,USB_CDC_EP_BULK_IN,
                  &CardDataBuffer[0], 0x10);
                   phpalI14443p3a_Sw_HaltA(&I14443p3a);

                   IsDataAvailable=0;


                       }
                  }
         }

    }

     Buzzer_Handle();

}
}

In the above code whenever I connect USB cable to my device the main card reading logic always fails
and without usb cable it works fine and send data over serial but the problem arises only when the USB cable is connected

what could be the isuue?
0 Kudos
Reply

1,987 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by crudo on Sun Sep 15 18:46:46 MST 2013
Can you post your code?
Maybe this is your problem: http://www.lpcware.com/content/forum/problem-with-subsequent-calls-to-writeep
0 Kudos
Reply