Segger Emwin Font Problem in ILI9341 for lpc1768??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segger Emwin Font Problem in ILI9341 for lpc1768??

1,231 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AkshayHV on Sun Nov 17 22:01:03 MST 2013
Hello
                i am interfacing a 3.2 inch TFT with LPC1768 ,the controller in the display is ILI9341. it is basically a spi interface and i am using a template code of NXP there i am not able to use all the fonts which are there in the library but some of the fonts are working fine for stings like "Hello World!" "www.kiel.com" and "www.segger.com" and for some of the fonts it is getting jumbled but for the number which runs from 0 to 9999 at the centre of the display is displaying each number two times for example instead of 0000 it is displaying "00000000" and for "1234" it is displaying "11223344".for which ever the font I use.please somebody help.


Thanks and Regards
Akshay H V
Labels (1)
0 Kudos
Reply
0 Replies