Seeking JTAG Programming Kit for F/W Updates

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Seeking JTAG Programming Kit for F/W Updates

1,198 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ACSDan on Tue Oct 22 07:33:58 MST 2013
We have built a device based on the LPC1114 chip. We flash the firmware to this via a 10 pin jtag cortex header, using a LPC LINK2. This works great for us in the lab environment however we are looking for a cost effective usb programming kit that would have very basic flash utility without debug functionality. We could develop this ourselves however we may not be making a massive amount of these devices to meet the MOQ of the large suppliers.

If anyone is aware of a suitable kit i would really appreciate your input.

Thanks in advance
Dan
Labels (1)
0 Kudos
Reply
1 Reply

1,188 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tha on Tue Oct 22 12:54:46 MST 2013
Segger have stand alone flash programmers:

http://www.segger.com/production-tools.html
0 Kudos
Reply