Secure booting from LPC18Sxx internal flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure booting from LPC18Sxx internal flash

1,013件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tnp353 on Thu Jan 28 09:06:46 MST 2016
The LPC18xx User Manual has a boot flow chart for encrypted images on flashless parts (Fig 27), but not for encrypted images on chips with internal flash. Figure 27 does make a little note about flash parts: "For parts with on-chip flash, the boot source is checked when the ISP pin is pulled LOW." However, that doesn't specify how the encrypted image in internal flash is handled once the bootloader determines the boot source is internal flash.

Is the encrypted image stored in internal flash decrypted in total to SRAM like for flashless parts? Or is the encrypted image in flash decrypted on-the-fly from flash as needed?

-Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

990件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Fri Jan 29 02:13:08 MST 2016
It is not decrypted on the fly. It is a similar process for internal and external flash.
0 件の賞賛
返信