Secure Boot Supported ARM MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Boot Supported ARM MCU

3,134件の閲覧回数
akaradag
Contributor II

Hi NXP technical support team,

I am looking for secure boot supported ARM MCU with features in below,

  - RSA-4096 bit public keys

  - x509 cert format support

  - sha256 hash function

  - OTP or PFR storage support

I see a few products (i.e. LPC5500), but cannot compare them. Could you please assist me to see all options with comparing of secure boot features... like a table

 

#mcu #secureboot #32-bit-arm #RSA-4096-#sha256

best regards, Anil

 

 

0 件の賞賛
返信
4 返答(返信)

3,086件の閲覧回数
akaradag
Contributor II

Hi @Alice_Yang ,

Thanks for your quick answer. There is a capability on NXP website to compare products. But, secure boot features are not in the property list NXP gives.

I can see details via checking data-sheet of the each family one by one. There might be ann internal method that creates a comparison table with all possible options. Can you do?

 

0 件の賞賛
返信

3,055件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @akaradag 

LPC55S6x/2x/1x/0x and LPC55s3x all support secure boot, and part number without "S" doesn't suport it. About Secure boot, LPC55S6x/2x/1x/0x is same, there is some difference for lpc55s3x.

There is a security feature comparison table:

 
 

Alice_Yang_2-1688720360687.jpegAlice_Yang_2-1688720360687.jpeg

 

BR

Alice

 

3,048件の閲覧回数
akaradag
Contributor II

many many thanks for this is a valuable support  

0 件の賞賛
返信

3,112件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @akaradag 

 

What do you want to compare, the four parts you list? We can not compare them, because they are not the same class, responsible for different functions, you can google them to know detail.

Secure boot of lpc55sxx use all the functions you mentioned. about secure boot, you can have a look at chapter 7 of UM11126.

 

BR

Alice

 

0 件の賞賛
返信