Sample code or documents for USB Host

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sample code or documents for USB Host

跳至解决方案
3,216 次查看
yasushiaoyama
Contributor I

Hi,

 

I’m developing USB host function for LPC4337 (Evaluation board OM13070).

But I cannot find out sample codes nor documents to help to make USB host function.

.

I download “lpcopen_3_01_lpcxpresso_nxp_lpcxpresso_4337”.  There are many USB device sample code in it, but no sample about USB host.

 

I read USB ROM stack 1.0 document, but all API seems to be for developing USB device.

 

I’d really appreciate if somebody help me.

 

Thanks,

 

Yasushi

0 项奖励
回复
1 解答
2,841 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi Aoyama,

    I find in the old lpcopen for MCBLPC4357, there has some USB host code, so you can refer to that code.

   It seems you are using LPCXpresso IDE, then I attach the sample code for your reference.

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,841 次查看
yasushiaoyama
Contributor I

Thank you very much, Kerry,

 I also found "lpcopen_2_20_lpcxpresso_nxp_lpcxpresso_4337" still has similar USB host code.  These code seems to be removed from ver 3_xx.  I checked release note of lpcopen_3_xx, but there is no description about removing USB host

 code.

 Any way your advice is helpful for me. 

Yasushi Aoyama

0 项奖励
回复
2,841 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi,

   Yes, I also find the 3.xx removed the host code, that's why I give you 2.20 code.

   You can refer to the 2.20 code directly.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,842 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi Aoyama,

    I find in the old lpcopen for MCBLPC4357, there has some USB host code, so you can refer to that code.

   It seems you are using LPCXpresso IDE, then I attach the sample code for your reference.

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复