Sample code or documents for USB Host

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample code or documents for USB Host

ソリューションへジャンプ
3,300件の閲覧回数
yasushiaoyama
Contributor I

Hi,

 

I’m developing USB host function for LPC4337 (Evaluation board OM13070).

But I cannot find out sample codes nor documents to help to make USB host function.

.

I download “lpcopen_3_01_lpcxpresso_nxp_lpcxpresso_4337”.  There are many USB device sample code in it, but no sample about USB host.

 

I read USB ROM stack 1.0 document, but all API seems to be for developing USB device.

 

I’d really appreciate if somebody help me.

 

Thanks,

 

Yasushi

0 件の賞賛
返信
1 解決策
2,925件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi Aoyama,

    I find in the old lpcopen for MCBLPC4357, there has some USB host code, so you can refer to that code.

   It seems you are using LPCXpresso IDE, then I attach the sample code for your reference.

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,925件の閲覧回数
yasushiaoyama
Contributor I

Thank you very much, Kerry,

 I also found "lpcopen_2_20_lpcxpresso_nxp_lpcxpresso_4337" still has similar USB host code.  These code seems to be removed from ver 3_xx.  I checked release note of lpcopen_3_xx, but there is no description about removing USB host

 code.

 Any way your advice is helpful for me. 

Yasushi Aoyama

0 件の賞賛
返信
2,925件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi,

   Yes, I also find the 3.xx removed the host code, that's why I give you 2.20 code.

   You can refer to the 2.20 code directly.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,926件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Yasushi Aoyama,

    I find in the old lpcopen for MCBLPC4357, there has some USB host code, so you can refer to that code.

   It seems you are using LPCXpresso IDE, then I attach the sample code for your reference.

pastedImage_1.png

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信