Sample Code for Keyboard wedge functionality using USB HID on NXP LPC2146

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample Code for Keyboard wedge functionality using USB HID on NXP LPC2146

1,896 Views
RussellPead
Contributor II

We are trying to implement Keyboard wedge functionality using USB HID interface on NXP’s LPC2146 based module. We would like to get some information on how it can be achieved. If there are any sample application or documentation which we can refer to understand the USB HID driver for LPC2146, please provide us the links.

Labels (2)
0 Kudos
Reply
1 Reply

1,706 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Russell,

You could take a look at the following link:

http://www.keil.com/download/docs/306.asp

 

Additionally, if you are developing a new USB-based application, it is recommended considering a newer LPC or Kinetis LPC microcontroller based on Cortex M4/M0+, as the LPC2xxx family is now legacy.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply