Sample Code for Keyboard wedge functionality using USB HID on NXP LPC2146

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample Code for Keyboard wedge functionality using USB HID on NXP LPC2146

1,931件の閲覧回数
RussellPead
Contributor II

We are trying to implement Keyboard wedge functionality using USB HID interface on NXP’s LPC2146 based module. We would like to get some information on how it can be achieved. If there are any sample application or documentation which we can refer to understand the USB HID driver for LPC2146, please provide us the links.

ラベル(2)
0 件の賞賛
返信
1 返信

1,741件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Russell,

You could take a look at the following link:

http://www.keil.com/download/docs/306.asp

 

Additionally, if you are developing a new USB-based application, it is recommended considering a newer LPC or Kinetis LPC microcontroller based on Cortex M4/M0+, as the LPC2xxx family is now legacy.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信