SWD programming speed, adaptable?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SWD programming speed, adaptable?

1,459 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by patroklos.anagnostou on Thu Nov 28 02:06:17 MST 2013
I am using just the LPC Link side of a LPC1115 Lpcxpresso board, trying to program via SWD a LPC11E37 target, in custom hardware.
The default programming speed is too high for my setup (there are couplers on the path) and by analyzing SWD protocol, I see that the ACK is not transmitted well because of clock delay.
Is it possible to adapt LPCLink's SWD speed through their LPCxpresso IDE?
If not, what similar programmer would do the job in lower rate? E.g. LPC-Link2?
Thank you for the support
标签 (1)
0 项奖励
回复
1 回复

1,338 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Nov 28 02:51:36 MST 2013
Link and Link2 doesn't allow to change speed.

See: Reducing wire speed

http://support.code-red-tech.com/CodeRedWiki/MultipleJtagDevices?highlight=%28speed%29

Note : This above wire speed information only relates to connections using RedProbe(+). LPC-Link only supports fixed wire speeds. 
0 项奖励
回复