STOP ALL INTERRUPTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

STOP ALL INTERRUPTS

1,206件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 02:36:43 MST 2015
Hello,

It would be possible to stop all interrupts using some register? Or I need to stop all enabled source interrupts and when I need to enable these to manage the source interrupts one by one?
I would like to know it because I am using the IAP commands to use the flash.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,196件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 03:24:07 MST 2015
You are OK!!
Thanks.
0 件の賞賛
返信

1,196件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Mar 18 03:05:30 MST 2015
What's wrong with  __disable_irq()  :quest:
0 件の賞賛
返信