STOP ALL INTERRUPTS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

STOP ALL INTERRUPTS

1,235 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 02:36:43 MST 2015
Hello,

It would be possible to stop all interrupts using some register? Or I need to stop all enabled source interrupts and when I need to enable these to manage the source interrupts one by one?
I would like to know it because I am using the IAP commands to use the flash.
标签 (1)
0 项奖励
回复
2 回复数

1,225 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Mar 18 03:24:07 MST 2015
You are OK!!
Thanks.
0 项奖励
回复

1,225 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Mar 18 03:05:30 MST 2015
What's wrong with  __disable_irq()  :quest:
0 项奖励
回复