SSP issue on LPC4088 Embedded Artists Dev Kits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SSP issue on LPC4088 Embedded Artists Dev Kits

1,514件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lenguyen on Mon Jan 20 08:37:44 MST 2014
Hi,

I configure SSP1 on LPC4088 dev kits using LPCOpen v1.03 to talk to TI ADC ADS8332 using SPI protocol. I can not get it to work. Here's couple information that we've seen so far. Both signals of Clock, MOSI from master (LPC4088) are good, however there is nothing from MISO, also chip select is low all the time. we also checked the documents and LPCopen code, there is a big discrepancy between LPCOpen and hardware configuration that on board schematic the SPI-SEL is GPIO69 and it's mapped to P2.14 however in Board_SSP_Init() function configures as P5.3.

Am I missing anything ?

Any input is very appreciated.

Thanks
LN
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,357件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Mon Jan 27 10:47:28 MST 2014
Hi, LN,
Please double check your pin configuration.
On EA 4088, SSP1 is P0.7, P0.6, P0.8 and P0.9 with LPCOpen V1.03 code. No signal is related with P2.14.
SSP2 is P5.2, P5.3, P5.1 and P5.0 with the LPCOpen V1.03 code.
Thanks,
0 件の賞賛
返信

1,357件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Sat Jan 25 10:42:25 MST 2014
Thanks LN. We will double check the LPC code and get back to you.
0 件の賞賛
返信