SSP Slave Transfer on Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SSP Slave Transfer on Interrupt

ソリューションへジャンプ
2,166件の閲覧回数
jamesm
Contributor II

Hello,

I have an 8 channel ADC which has the following output:

There is a continuous SCLK at 4MHz, though there is only a burst of 32 bytes of data once per ms.

Once per ms, a DataReady line goes inactive for one SCLK cycle (250ns) and then returns to active. Unfortunately, it stays active after the data is transmit.

When DataReady goes active, SCLK goes high, transferring first bit onto bus. This bit needs to be sampled when SCLK goes low 125ns later.

Is there a way to capture this data directly with an LPC1769?

If I try to use an interrupt on the DataReady signal to begin a DMA transfer, I cannot get the transfer started in time as it takes almost 2us to get the interrupt going and the first bit needs to be sampled 125ns after the DataReady goes active.

If I try to run the DataReady signal into the SSEL pin, and set the DMA transfer up each time I get new data, it runs more or less continuously because the SSEL signal is staying low after the data is transmitted.

Is there some way to set up a DMA transfer based on the falling edge of the SSEL pin instead of the level of that pin so that it only happens once each time the SSEL goes up and down? Or is there a way to get the DMA transfer started fast enough to get the first bit within 125ns?

Thanks for any insight - James

0 件の賞賛
返信
1 解決策
2,030件の閲覧回数
jamesm
Contributor II

Thank you Ping

I have learned that I should be able to use a Timer to detect the DataReady signal and generate a Match, triggering the DMA. I almost have this working and have asked a new and much more complete question about it yesterday. It is called "Cannot Trigger DMA with Timer Match". Thank you for your help.

James

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,031件の閲覧回数
jamesm
Contributor II

Thank you Ping

I have learned that I should be able to use a Timer to detect the DataReady signal and generate a Match, triggering the DMA. I almost have this working and have asked a new and much more complete question about it yesterday. It is called "Cannot Trigger DMA with Timer Match". Thank you for your help.

James

0 件の賞賛
返信
2,030件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi James Massey,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

I've had some queries which needs your explanation.

1. In your design, the LPC1769 work as the slave and using the SSP module to receive the data from the master side, doesn't it right?

1. Can you tell which communication protocol you select?

2. According to your statement, the DataReady is equal to the SSEL which determine the start and shutdown the transmission. so I think the SSP included DMA feature is the better choice.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信