SSP Demo Example is failing at buffer verify for LPC 1837

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SSP Demo Example is failing at buffer verify for LPC 1837

1,640 Views
srikanthmediset
Contributor I

Hi,

    I am using LPC 1837 controller and using Expresso IDE.I am trying to run the SSP demo example for SPI on two LPC boards.Following are my connections for that

Board 1:

    =>Configured as Master.

    => P1.5 as SSEL which is connected to SSEL on other LPC 1837 board.

    => PF.4 as SCK1 which is connected to SCLK on other LPC 1837 board.

    => P1.4 as MOSI which is connected to MISO on other LPC 1837 board.

    => P1.3 as MISO which is connected to MOSI on other LPC 1837 board.

Board 2:

    =>Configured as Slave.

    => P1.5 as SSEL

    => PF.4 as SCK1

    => P1.4 as MOSI 

    => P1.3 as MISO 

     When I am running the demo application on both the boards and I am getting always buffer_verify() failure.Do I need to do anything beyond these connections or anything to be added in the code.

Regards

srikanth.

Labels (1)
0 Kudos
Reply
1 Reply

1,526 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Srikanth Medisetty,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer the attachment which contains the master_SSP and slave_SSP demo。
Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply