SPIFI vs SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPIFI vs SPI

3,530件の閲覧回数
TEMCEFF
Contributor IV

What is difference between  Interfacing of External Serial flash using SPIFI and SPI? what are the Advantages of using SPIFI over SPI?

ラベル(1)
0 件の賞賛
返信
1 返信

3,380件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Muralidhar,

The SPIFI focuses on interface with SPI flash only, the SPI is an interface which can connect to a lot device including flash.

Regarding the difference, the normal SPI module has 4 signals: /SS, SCLK, MOSI and MISO signals, the /SS, SCLK and MOSI are driven by SPI master, the MISO signal is driven by slave. The normal SPI can interface with single I/O SPI flash.

The SPIFI interface includes /SS, SCLK and dual/quad/8 data lines, the data lines are bidirectional, they can input or output. In general, the Data0 line is command line, it transfer command to flash in the first phase, then the spifi module transfers address by all data lines or just data0 line, then spifi can transfer data depending on the command.

The SPIFI can generate the timing to access spi flash.

I attach the RM of SPI flash, pls refer to the doc to know the required timing of spi flash.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信