SPIFI cache and capabilities

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPIFI cache and capabilities

1,209件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cb03scs on Tue Oct 21 04:43:03 MST 2014
Currently we are using the LPC4370 for a project and there were some unanswered questions about the SPIFI:

In the User-Manual is the sentence: "Built-in cache to give high-performance code execution."
But how big is the cache really? 8B, 32B, ..., 1kB, ...?
How long is one cache line? 8B, 16B, ...?
What is the clock of the cache? is it the same as the whole SPIFI module or is it clocked with the AHB bus speed?

And some other question regarding the compatibility of the SPIFI module:
Is it compatible with SD-Cards? Could I remove the 4MB Flash on the evaluation board and attach an SD-Card without the need of a special boot loader? (That I'd be unable to access the whole SD-Card at once or even at all is not important to me.)

Are there some Documents on the NXP Homepage that I have not found yet regarding these questions?

If someone could answer these questions that would be terrific...

Thank you
ラベル(1)
0 件の賞賛
返信
1 返信

1,170件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cb03scs on Wed Nov 05 05:07:31 MST 2014
Well I got an answer from the Tech Support of NXP:

Hi Chris,
We do not disclose this information, however there is sufficient cache to perform execution in place with good execution performance.
0 件の賞賛
返信