SPIFI boot rom device support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPIFI boot rom device support

1,974件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rockyh on Wed Jul 23 07:45:54 MST 2014
Hi,
Where can I find the list of SPI flashes that the SPIFI boot ROM code can boot from? In particular, I'm interested if booting is possible with ST M25P80 standard SPI flash.  Has anyone used this with success?  If we program SPIFI with Keil ULINK2 everytime, the code runs fine, but we can't seem to boot up from SPIFI.

Thanks for any info you can provide.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,940件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jul 30 10:50:25 MST 2014
Hi rockyh,
Yes. We are compiling the list and will be available at lpcware.com.
0 件の賞賛
返信

1,940件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rockyh on Wed Jul 30 08:06:02 MST 2014
Thank you, mc.  For the future, it would be good to know a list of devices the Boot ROM supports. Does NXP have a list?
0 件の賞賛
返信

1,939件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Jul 25 12:36:48 MST 2014
Hi rockyh,
Yes it boots from M25P80. Use attached project.
0 件の賞賛
返信