SPIFI affects UART?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPIFI affects UART?

1,644 次查看
tlenek
Contributor I

I have a little problem, which I identified as SPIFI affection on UART. In one part of my code I initialize the SPIFI interface using spifilib. In spifiPrvDevGetID function (which is a part of a function stack) there are instructions that read and write data directly from SPIFI controller adresses. Further in my code I send information through UART. But it causes Bus Fault while debugging. Removing instructions from spifiPrvDevGetID function solves the problem, but these commands are necessary to initialize SPIFI correctly. What could cause such kind of problems? Do you know any solution to that problem?

 

My MCU is LPC4330.

标签 (1)
标记 (5)
0 项奖励
回复
1 回复

1,493 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tomasz,

Could you share your project so we can reproduce the issue on our side?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复