SPIFI-NXP-MICROCONTROLLERS: LPC SPIFI Peripheral - Cypress S25FL064LABNFI013

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPIFI-NXP-MICROCONTROLLERS: LPC SPIFI Peripheral - Cypress S25FL064LABNFI013

ソリューションへジャンプ
1,867件の閲覧回数
danielgull
Contributor IV

Hi, I am using the LPC SPIFI Peripheral Library:

MCUXpressoIDE_11.2.0_4120\ide\Examples\Flashdrivers\NXP\LPC5460x\LPC5460x_lpcspifilib_driver.zip\LPC5460x_SPIFIdriver_Generic\lpcspifilib

Will there be any updates to this library to add new devices?

Will NXP add the SPIF device "Cypress S25FL064LABNFI013" to this library?

If yes, when will this update be available?

Many Thanks

Dani

0 件の賞賛
返信
1 解決策
1,850件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @danielgull,

Until now there's is no news about this device being added to the library but you can modify the library add the support for new devices. In the following presentation, there is some consideration to modify the SPIFI library.

It looks like this memory support the same serial command structure as the one already added to the library (S25FL-P), I will suggest looking at the commands used by this memory and also look in the SPIFI examples found in the SDK.

Best Regards,

Alexis Andalon

元の投稿で解決策を見る

1 返信
1,851件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @danielgull,

Until now there's is no news about this device being added to the library but you can modify the library add the support for new devices. In the following presentation, there is some consideration to modify the SPIFI library.

It looks like this memory support the same serial command structure as the one already added to the library (S25FL-P), I will suggest looking at the commands used by this memory and also look in the SPIFI examples found in the SDK.

Best Regards,

Alexis Andalon