SPIFI Flash during programming?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPIFI Flash during programming?

1,654件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thiapalm on Thu Apr 14 08:54:54 MST 2016
Hello,

We have an application that will load some pre-defined images from SPIFI Flash device to use during run time. Nowadays we run one project just to save the images on the SPIFI Flash, and another with the final code that will read it.

Is it possible to upload code to a SPIFI external Flash device during programming (via Linker script)? So we avoid this two step approach?

If so, is there any documentation about it?

Thanks
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,611件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,611件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Fri May 06 12:54:14 MST 2016
You don't mention which tools you are using. On the assumption you are using lpcxpresso, then look at the FAQs where the is information about linker scripts and placing data in specific sections.

P.s. This is a community forum not a support site. If you want support, ask for it on the main NXP site.
0 件の賞賛
返信

1,611件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thiapalm on Fri May 06 10:26:50 MST 2016
The support provided by NXP for its products is outstanding....

One month passed and not a single person from NXP replied.

We simply can't deal with such long response time....
0 件の賞賛
返信