SPI with DMA support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI with DMA support

1,687 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by naveed_33 on Thu Jan 03 03:55:00 MST 2013
Hello,
I am new to nxp controller . i wanted to ask that is it possible to operate SSP with 16 bit DMA . because it does not work like that with ST controller(only 8 Bit supported there)
标签 (1)
0 项奖励
回复
3 回复数

1,656 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by naveed_33 on Tue Jan 15 14:45:34 MST 2013
thanks for the help
0 项奖励
回复

1,656 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Fri Jan 11 17:02:14 MST 2013
DMA on the LPC18xx supports 8, 16, and 32-bit transfers and it can be used with the SPI which supports from 4-bit to 16-bit frames.

-Dave @ NXP
0 项奖励
回复

1,656 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by naveed_33 on Thu Jan 03 03:58:09 MST 2013
i am using NXP LPC 1857
0 项奖励
回复