SPI issues in the LPC54018

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI issues in the LPC54018

6,079 次查看
VIGNESH_BABU
Contributor II

Hi,

we are working with the customized LPC54018 Micro-controller interface with the TFT_DISPLAY(ST7789V).Actually our display was working properly in the NON-XIP Project.While we are  working with XIP Project where we getting the clock data but the display doesn't shown the correct data/ didn't get refreshed?

标记 (1)
0 项奖励
回复
11 回复数

5,957 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can download the code to spifi flash and check the SYSCON register to know the LCD driving clock, SPIFI driving clock frequency,cpu clock frequency.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1672113496989.png

 

0 项奖励
回复

5,908 次查看
VIGNESH_BABU
Contributor II

Hi Xianjun Rong;

In XIP and NO-XIP both the frequency are configured as same.But the execution speed is low while compare with the NO-XIP. what is the reason behind to slow down the speed of execution in XIP Mode.Is there is any other option to increases the clock speed in XIP Mode.

I was attached the images of frequency of XIP and NON-XIP and also attached the project file of XIP and NO-XIP in ZIP File.

 

NO-XIPNO-XIP  XIPXIP

0 项奖励
回复

5,855 次查看
VIGNESH_BABU
Contributor II

Is there is anyway to increases the frequency in the XIP mode?

 

0 项奖励
回复

5,918 次查看
VIGNESH_BABU
Contributor II

Is there is any other option to check?Please Kindly Reply us.

 

0 项奖励
回复

5,945 次查看
VIGNESH_BABU
Contributor II

Hi Xianjun Rong;

1.I was download the SPIFI flash and set the clock as 96MHz.

2.And we are not used the LCD Driving clock because TFT was connected with the FLEXCOMM 9.And the clock was set as 96 MHZ.

3.Then the CPU Clock was in 12 MHz.

4.Finally there is no change in speed of the display same as before.

0 项奖励
回复

6,069 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the data sheet of TFT_DISPLAY(ST7789V), it is three wires spi interface, you said that the display was working properly in the NON-XIP Project, but did not work when you run the project in XIP.

Pls check the following items:

1)pls check if the display spi signals are overlapped with the spifi siganal which is connected to spifi flash.

2)Pls try to create a LED toggling example in XIP mode(toggling a LED in a fixed period Timer ISR), and check if the LED can toggle in XIP mode.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复

6,044 次查看
VIGNESH_BABU
Contributor II

Hi XiangJun Rong,

I was worked with LED Toggle examples in the LPC54018 Controller. Where the LED was worked very well and there is no overlapped in the SPI signals

0 项奖励
回复

6,037 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is my guess, Running in internal SRAM is faster that that of running in spifi flash, which leads to the fact that the core can not update the data in display buffer in time. If it is the case, pls simplify the code to reduce the core load.

BR

XiangJun Rong

 

0 项奖励
回复

6,020 次查看
VIGNESH_BABU
Contributor II

Hi XiangJun Rong,

According to your suggestion I was reduce the core load to flash the code in TFT Display.I got the data in my display.But the speed quite low compare to NON-XIP. I was attach the Video file of XIP and NON-XIP Execution in display.

0 项奖励
回复

5,993 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have played your *.mp4 file, when you run in XIP mode, it appears that core clock is very low compared with the running in on-chip RAM, pls check the core clock, LCD driving clock and pixel clock frequency in XIP mode.

BR

XiangJun Rong

0 项奖励
回复

5,970 次查看
VIGNESH_BABU
Contributor II

How to check the  LCD driving clock and pixel clock frequency in XIP mode?.

0 项奖励
回复