SPI frequency problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI frequency problem

877 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Coralicious on Mon May 27 03:48:43 MST 2013

Hello guys.


I'm working with master-slave SPI communication by interruption (SPI1_IRQHandler). It was working fine with a frequency of 2 MHz, but I got to change the frequency because of the electrical noise to 100 kHz. And now, it doesn't work because when the slave is sending 0x00, master is reading 0xFF.


 


How could I solve this?


Thanks

标签 (1)
0 项奖励
回复
0 回复数