SPI continuous chip select on LPC54608 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI continuous chip select on LPC54608 MCU

2,885 Views
Jetcitycowboy
NXP Employee
NXP Employee

Is the only way to get a continuous chip select is define the pin as a GPIO and set the state of the pin? 

Labels (2)
2 Replies

2,550 Views
soledad
NXP Employee
NXP Employee

Hi,

This device has four Slave Select input/outputs with selectable polarity and flexible usage.

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,550 Views
hlsamts
Contributor III

If someone asks you about the color of an apple, are you going to tell her/him that a banana is yellow?!

No.

Your response does not answer the question.