SPI continuous chip select on LPC54608 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI continuous chip select on LPC54608 MCU

2,898件の閲覧回数
Jetcitycowboy
NXP Employee
NXP Employee

Is the only way to get a continuous chip select is define the pin as a GPIO and set the state of the pin? 

ラベル(2)
2 返答(返信)

2,563件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

This device has four Slave Select input/outputs with selectable polarity and flexible usage.

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,563件の閲覧回数
hlsamts
Contributor III

If someone asks you about the color of an apple, are you going to tell her/him that a banana is yellow?!

No.

Your response does not answer the question.