SPI Transmission Data Corruption on LPC1768 Using SSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Transmission Data Corruption on LPC1768 Using SSP

Jump to solution
1,765 Views
AkshayNaik1907
Contributor II

 

Hi,

I am working with the LPC1768 SSP peripheral in SPI master-slave mode. I am facing an issue with transmitted data when using ISR-based SPI transfers. Here’s the behavior I observe:

Expected behavior:

  • MOSI should send: 11 22 33 44 55 66 77 88 99

  • MISO should receive: 01 12 23 34 56 67 78 89
    (The first byte from slave is 01 since the slave initially has no data.)

Observed behavior:

  • When I run the code continuously, MOSI is transmitted incorrectly in some cases. For example, the last bytes appear corrupted or repeated, and only 23 bytes are sent instead of 32. and some bytes are meant to sent 0x55 but its transmitting 0x00.

  • When I put breakpoints and step through, the data is transmitted correctly.

Setup:

  • Using SSP0 on LPC1768

  • Interrupts enabled for TX and RX: SSP0_IMSC = (1<<2) | (1<<3)

  • Data width: 8-bit

  • ISR-based, polling-free transfer

 

Questions:

  1. Has anyone seen similar SPI transmission issues on LPC1768 where data gets corrupted or incomplete during continuous ISR-based transfers? Could this be related to FIFO timing, clock phase settings, or ISR handling?

  2. Is there an errata or known issue with LPC1768 SSP that could cause this behavior?

  3. Could this also be related to the board itself or how it handles SPI signals?

I have attached the ISR code file.

Thank you

0 Kudos
Reply
1 Solution
1,703 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @AkshayNaik1907 

Thanks for your question.

1)What SPI slave device is connected to the LPC1768?
2)Please use a logic analyzer to measure and check whether the signals are correct.
3)Additionally, please try lowering the SPI speed to see if it improves functionality.

Thank you.

 

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,704 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @AkshayNaik1907 

Thanks for your question.

1)What SPI slave device is connected to the LPC1768?
2)Please use a logic analyzer to measure and check whether the signals are correct.
3)Additionally, please try lowering the SPI speed to see if it improves functionality.

Thank you.

 

BR

Alice

0 Kudos
Reply