SPI Slave configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI Slave configuration

2,665 Views
jinu_mohan
Contributor I

Hi ,

im using LPC xpresso55S28 board configured Flexcom 7 as spi master .

i need to control 4 slave devices in SPI im not able to create 4 chipselect in IDE pinmuxing tool

is that possible to create 4 chip select option in LPC xpresso55S28 

@Alice_Yang 

0 Kudos
Reply
3 Replies

2,642 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I checked the Datasheet, and this mentions the following.

  • Up to Four Slave Select input/outputs with selectable polarity and flexible usage

I reviewed the Datasheet in the pinout has SPI Slave Select 0/1/2/3, I recommend using the MCU config tool to set this more easily. If you need more information please let me know.

Best regards,
Pavel

0 Kudos
Reply

2,651 Views
Badman
Contributor I

I don't know how many controllers lpc has SPI. You can use software ChipSelect using GPIO. 

0 Kudos
Reply

2,587 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I created a case to continue to help you, 00475476, If you need more information I will contact you in the other case.

Best regards,
Pavel

0 Kudos
Reply