SPI SD-Card on LPC5516

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI SD-Card on LPC5516

961 Views
Christian42
Contributor I

Hello everyone,

I am currently working on a project with a LPC556JB100 chip and I am trying to get sd card support via SPI to work. I am a bit lost at the moment as there is no option in the configurator for sd card.

I already configured the SPI and included the FatFS middleware. The configurator just won't let me choose SPI SD card as MSDK adaption configuration. My only options are USB and RAM disk. I have also not been able to find a way to include a sd card driver which is working for this chip since the chips SDK does not offer it.

Current SDK: SDK_2.x_LPC5516 v2.13.0

Can anyone point me in a direction as to where I can find a working method to get a SPI SD card working with FatFS on the LPC5516?

Thanks in advance!

Labels (2)
0 Kudos
Reply
0 Replies