SPI Rx interrupt not generated in LPC55S28 if we disable SPI Tx interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Rx interrupt not generated in LPC55S28 if we disable SPI Tx interrupt

3,283 次查看
rahulshah
Contributor I

Hello,

I am using LPC55S28 EVM board. i have 2 LPC55S28 EVM boards and  i tried to run SPI master slave SPI SDK example on that.

On Baord-1, i have flashed "lpcxpresso55s28_SDK_spi_interrupt_b2b_master" SDK example code.

And on Board-2 , i have flashed "lpcxpresso55s28_SDK_spi_interrupt_b2b_slave" SDK example code.

I have connected pins as described in Readme of the SDK example code. Readme also attached with this case.

Without any change in code everything works fine , data send from master device and received at slave device. Again same received data send from slave device and received properly at master side.

 

But Now i want to only receive data at slave side. So if i disable Tx -interrupt at slave side then i cannot receive data in slave device.
 

In "spi_interrupt_b2b_slave.c" file of SDK example code , in main functoion i have disabled tx interrupt as below :

Original : SPI_EnableInterrupts(EXAMPLE_SPI_SLAVE, kSPI_RxLvlIrq | kSPI_TxLvlIrq);

Changed to : SPI_EnableInterrupts(EXAMPLE_SPI_SLAVE, kSPI_RxLvlIrq);

 

So after that if Master sends data over SPI , then Rx interrupt not generated at slave side and code not goes in Irq function.

I have attached SPI master-slave example code with this case.

Can anyone explain me this behavior. How i solve this issue?

Regards,

Rahul Shah

 

 

标签 (1)
0 项奖励
回复
4 回复数

3,271 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Rahul Shah,

ISP must send data, at the same time it can received data.

You disable slave Tx interrupt, from the SDK slave code, we can see it can't run into interrupt at start, 

so won't run slave Tx funciton " SPI_WriteData(EXAMPLE_SPI_SLAVE, (uint16_t)(srcBuff[BUFFER_SIZE - txIndex]), 0);".  

You can add this function in main() to test.

 

Regards,

Alice

0 项奖励
回复

3,261 次查看
rahulshah
Contributor I

Hi Alice_Yang,
Thanks for your reply.

So my main question is if i disable tx-interrupt from "SPI_EnableInterrupts" then i am never going in ISR. is it right?
Because if i enable Tx-interrupt , then ISR calling again and again. So i want ISR only calling when slave recieves the data over SPI otherwie ISR should not call.

So how i only receive data from ISR function without enabling Tx-interrupt.

-Regards,
Rahul Shah

0 项奖励
回复

3,255 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello,

So my main question is if i disable tx-interrupt from "SPI_EnableInterrupts" then i am never going in ISR. is it right?

->> No.

So how i only receive data from ISR function without enabling Tx-interrupt.

->>You can disable Tx-interrupt, while you need send data to master, at the same time, slave can received data automatically. 

And if you just want to SPI slave receive, not send, you can try to the function of ignore transmit data :

(UM11126, P673)

 

spi.jpg

Please also pay attention:

"To set-up a slave SPI for receive only, the control bit settings must be pushed into the
write FIFO to become active. Therefore, at least one write to the FIFOWR data bits must
be done to make the control bits active"

Regard,

Alice

0 项奖励
回复

3,195 次查看
rahulshah
Contributor I

Hi ,

I have added TXIGNORE=1 as follows (1<<23):

EXAMPLE_SPI_SLAVE->FIFOWR= (0x01|
((uint32_t)SPI_FIFOWR_LEN(kSPI_Data8Bits) |
(SPI_DEASSERT_ALL & (~SPI_DEASSERTNUM_SSEL(0)))) | (1 << 23)) ;

Also i have disabled tx-interrupt and disabled data sending from slave side from ISR  as follows :

// if ((SPI_GetStatusFlags(EXAMPLE_SPI_SLAVE) & kSPI_TxNotFullFlag) && (txIndex > 0U))
// {
// SPI_WriteData(EXAMPLE_SPI_SLAVE, (uint16_t)(srcBuff[BUFFER_SIZE - txIndex]), 0);
// txIndex--;
// }

After that i am not getting data properly from master:

Master sends : [0,1,2,3,4,5,6,7,8,9,10,11,12,13..........63]

Slave receives : [0,0,0,0,1,0,0,0,2,0,0,0,3,0,0,1....]

If i enable data sending from slave from ISR , then everything works fine.

I have added FIFOWR logic in init function so is that TXIGNORE bit set (1<<23) in FIFOWR is ok?

Regards,

Rahul Shah

 

 

0 项奖励
回复