SPI ROM Driver on LPC8xx?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI ROM Driver on LPC8xx?

2,197件の閲覧回数
thomasjohansen
Contributor I

 In a prev. thread a NXP memeber wrote 'it wasn't recommended to use the SPI ROM driver of the LPC8xx'.

Is this still the case? and why?

 

Thomas

0 件の賞賛
返信
3 返答(返信)

1,982件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Thomas Johansen,

The fig 1 has illustrated the SPI API calls and you can use these API calls directly if the API calls meet your requirement.

2016-09-26_13-54-12.jpg

                                                                 Fig 1


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,982件の閲覧回数
thomasjohansen
Contributor I

Hi, 

Thanks for reply. This 3 year old post a NXP support memeber state that its usage is NOT recommended?

[LPC8xx] SPI ROM driver, missing DMA_HANDLE_T specification | www.LPCware.com  

Thomas

0 件の賞賛
返信

1,982件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Thomas Johansen,

In the reference manual, you can find a lot information about using the SPI ROM API calls.

In my opinion, you can have a try.

If you have any question about it, you can feel free to contact with me.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信