SPI COMMUNICATION ON LPC1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI COMMUNICATION ON LPC1768

4,329件の閲覧回数
akshaybuchake
Contributor I

I am doing communication in MCP3202 and LPC1768 via SPI(interrupt based) but i am getting data 0X00FF only....I am attaching code here

0 件の賞賛
返信
2 返答(返信)

2,714件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

In order to isolate the issue (hardware or software) could you please test the LPCopen spi examples?

LPCOpen Software for LPC17XX|NXP 

Have a great day,

Sol

 

 

 

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,714件の閲覧回数
akshaybuchake
Contributor I

Hello 

Thanks for early reply

But your solution to use NXP softwere  is not possible for me...because all the drivers other than SPI

I have to change according to that libraries....can you suggest the bug in my code?(for your verification of hardware one code with Memory card interfacing using SPI is working properly but ADC communication is not proper)... 

0 件の賞賛
返信