SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SHA 256 Calculation LPC55S28 - BUG in fsl_hascrypt.c ?

Jump to solution
2,774 Views
Baur_phg
Contributor I

I have a few questions about the SHA function and the implementation in the FSL drivers fsl_hashcrypt.c.

I need the SHA checksum to check the firmware in the internal flash memory

I am currently using version 11 of the LPC55S28 SDK and the HASHCRYPT_SHA() function there

1. Is it possible to use a flash memory area directly as a source in register MEMADDR, according to the LPC manual only SRAM0 or SRAMX can be used, but the version with direct flash access is also suggested here in the forum, or does the flash data have to be copied to the RAM first? .

The calculation with the flash memory actually worked without any problems and also generated correct SHA checksums.

2. There seems to be a bug in the FSL drivers in the fsl_hashcrypt.c module. The functions of the SHA calculation, e.g. hashcrypt_sha_process_message_data, only evaluate the HASHCRYPT_STATUS_DIGEST_MASK but not HASHCRYPT_STATUS_ERROR_MASK in the event of an error, the drivers never come back and the watchdog strikes. This happens when trying to calculate the SHA of a deleted Flashpage, where the HASHCRYPT_STATUS_ERROR_MASK flag is set.

We are currently using the SDK version 11, but the query is also identical in version 12. The start address of the flash memory is aligned. (0x20000)

3. The SHA drivers do not check the length of the data, if more than the possible 2047 blocks 131008 bytes are specified, there is no error message but an incorrect SHA

It would be great if someone could help me with the issues.

Labels (1)
0 Kudos
Reply
1 Solution
2,721 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is the feedback from AE engineer:

"

As stated in UM, SHA engine can read from SRAM or flash.

xiangjun_rong_0-1676602560229.png

 

2. The root cause is LPC5500 flash cannot be read after erase operation. I have created a ticket to SDK team to improve this issue.

3. This is a SDK issue, the SDK driver doesn't check the length of the content. I have created a SDK ticket for the issue.

"

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
4 Replies
2,648 Views
Baur_phg
Contributor I

Thanks for the answer and the help,

In the UM register description of the memory address register MEMADDR, only the SRAM is specified, thats why i was a little bit confused

I modified the sha function and check the HW Error Flag, now it returns with Error Status if the Flash is not programmed.

now it works as expected

Thanks

0 Kudos
Reply
2,722 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is the feedback from AE engineer:

"

As stated in UM, SHA engine can read from SRAM or flash.

xiangjun_rong_0-1676602560229.png

 

2. The root cause is LPC5500 flash cannot be read after erase operation. I have created a ticket to SDK team to improve this issue.

3. This is a SDK issue, the SDK driver doesn't check the length of the content. I have created a SDK ticket for the issue.

"

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply
2,728 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Baur

Can you tell us the target application? The item is required by the AE team.

BR

XiangJun Rong

0 Kudos
Reply
2,751 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked AE  security team, I will answer your question after I get feedback.

BR

XiangJun Rong

0 Kudos
Reply