SGPIO synchronizing as a slave device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGPIO synchronizing as a slave device.

1,739件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Nickel on Tue May 10 02:59:15 MST 2016
Hi when used as a slave device it would seem the SGPIO has no mechanism to synchronize to the master device word / frame / LR clock. A bit of an oversight or have I missed something in the data sheet?

I have tried using a clock qualifier to gate the incoming clock to pull the data in line. This has mixed success and resync can take many frames.

Is there a way to reset the POS counter from an input pin perhaps, much like a standard external SPI peripheral?
ラベル(1)
0 件の賞賛
返信
1 返信

1,698件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信