SDRAM strange problem!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM strange problem!

ソリューションへジャンプ
2,497件の閲覧回数
behnamshakibafa
Contributor II

Hi everybody

I designed new PCB with exact same schematic with my avaluation board, but got in trouble with SDRAM.

the K4S511632 chip is used. I tried a test code. what I can see is that error in writing or reading with a constant pattern. I write data on all space, then the on reading, every 4 32bit data I read, one time has error and every time error is same. I wrote 0xBBCCDDEE and I read 0x0xBBCCBBCC!

Can any one help me on this?

     /* Writing */     
     for (i=0; i<SDRAM_SIZE/4; i++)
     {
       *char_wr_ptr++ = 0xEE;
       *char_wr_ptr++ = 0xDD;
       *char_wr_ptr++ = 0xCC;
       *char_wr_ptr++ = 0xBB;
     }

       /* Verifying */     
     wr_ptr = (uint32_t *)SDRAM_BASE_ADDR;
       for ( i= 0; i < SDRAM_SIZE/4; i++ )
       {
          if ( *wr_ptr != 0xBBCCDDEE )     /* be aware of endianess */
          {
                 /* byte comparison failure */
               err++;
          }
          wr_ptr++;
       }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Thanks

Behnam

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
2,299件の閲覧回数
avt
Contributor III

This forum is for LPC parts not Kinetis. Suggest that you post to a more appropriate forum.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,299件の閲覧回数
behnamshakibafa
Contributor II

Please help me on this dudes

0 件の賞賛
返信
2,300件の閲覧回数
avt
Contributor III

This forum is for LPC parts not Kinetis. Suggest that you post to a more appropriate forum.

0 件の賞賛
返信