SDRAM interfacing Problem with lpc4357

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM interfacing Problem with lpc4357

4,709件の閲覧回数
tintuthomas
Contributor I

Hi all,

I am trying to interface SDRAM - AS4C8M16SA from Alliance, with LPC4357 (LQFP208 package). I'm not familiar with EMC or SDRAM. I got the RAM get initialized. But ,I cannot successfully write beyond 64 bytes into it. My connection details and initialization code are given below.


SDRAM Details

  •     Alliance AS4C8M16SA
  •     128M - 8M x 16 bit , 2M word x 16-bit x 4-bank
  •     CAS Latency: 2, or 3
         Burst Length: 1, 2, 4, 8, or full page
         Burst Type:  Sequential or Interleaved
  •      4096 refresh cycles/64ms

Connections

SDRAM                            LPC4357

DQ0 - DQ15            EMC_D0 - EMC_D15

A0 - A11                   EMC_A1 - EMC_A12

BA0                          EMC_A13

BA1                          EMC_A14

RAS                         EMC_RAS

CAS                         EMC_CAS

CS                           EMC_DYCS0

WE                          EMC_WE

NC/RFU                   NC

LDQM                      EMC_DQMOUT0

UDQM                      EMC_DQMOUT1

CLK                          EMC_CLK0

CKE                          EMC_CKEOUT0

Note: EMC_A6, EMC_A7, EMC_A8 and EMC_A0 pins are connected to some pull-up circuits to select the ISP method. The connection picture is attached.

Code

void SDRAM_Init () {
    uint32_t pclk, temp;
    uint32_t tmpclk;
    TIM_TIMERCFG_Type TIM_ConfigStruct;
    
    /* Set up EMC pin */
    scu_pinmux(    1    ,    0    ,    MD_PLN_FAST    ,    2    );    //A5
    scu_pinmux(    1    ,    1    ,    MD_PLN_FAST    ,    2    );    //A6
    scu_pinmux(    1    ,    2    ,    MD_PLN_FAST    ,    2    );    //A7
    scu_pinmux(    1    ,    3    ,    MD_PLN_FAST    ,    3    );    //OE
    scu_pinmux(    1    ,    4    ,    MD_PLN_FAST    ,    3    );    //BLS0
    scu_pinmux(    1    ,    5    ,    MD_PLN_FAST    ,    3    );    //CS0
    scu_pinmux(    1    ,    6    ,    MD_PLN_FAST    ,    3    );    //WE
    scu_pinmux(    1    ,    7    ,    MD_PLN_FAST    ,    3    );//D0
    scu_pinmux(    1    ,    8    ,    MD_PLN_FAST    ,    3    );//D1
    scu_pinmux(    1    ,    9    ,    MD_PLN_FAST    ,    3    );//D2
    scu_pinmux(    1    ,    10    ,    MD_PLN_FAST    ,    3    );//D3
    scu_pinmux(    1    ,    11    ,    MD_PLN_FAST    ,    3    );//D4
    scu_pinmux(    1    ,    12    ,    MD_PLN_FAST    ,    3    );//D5
    scu_pinmux(    1    ,    13    ,    MD_PLN_FAST    ,    3    );//D6
    scu_pinmux(    1    ,    14    ,    MD_PLN_FAST    ,    3    );//D7
    scu_pinmux(    2    ,    0    ,    MD_PLN_FAST    ,    2    );//A13
    scu_pinmux(    2    ,    1    ,    MD_PLN_FAST    ,    2    );//A12
    scu_pinmux(    2    ,    2    ,    MD_PLN_FAST    ,    2    );//A11
    scu_pinmux(    2    ,    6    ,    MD_PLN_FAST    ,    2    );//A10
    scu_pinmux(    2    ,    7    ,    MD_PLN_FAST    ,    3    );//A9
    scu_pinmux(    2    ,    8    ,    MD_PLN_FAST    ,    3    );//A8
    scu_pinmux(    2    ,    9    ,    MD_PLN_FAST    ,    0    );//A0// changed as GPIO
    scu_pinmux(    2    ,    10    ,    MD_PLN_FAST    ,    3    );//A1
    scu_pinmux(    2    ,    11    ,    MD_PLN_FAST    ,    3    );//A2
    scu_pinmux(    2    ,    12    ,    MD_PLN_FAST    ,    3    );//A3
    scu_pinmux(    2    ,    13    ,    MD_PLN_FAST    ,    3    );//A4
    scu_pinmux(    5    ,    0    ,    MD_PLN_FAST    ,    2    );//D12
    scu_pinmux(    5    ,    1    ,    MD_PLN_FAST    ,    2    );//D13
    scu_pinmux(    5    ,    2    ,    MD_PLN_FAST    ,    2    );//D14
    scu_pinmux(    5    ,    3    ,    MD_PLN_FAST    ,    2    );//D15
    scu_pinmux(    5    ,    4    ,    MD_PLN_FAST    ,    2    );//D8
    scu_pinmux(    5    ,    5    ,    MD_PLN_FAST    ,    2    );//D9
    scu_pinmux(    5    ,    6    ,    MD_PLN_FAST    ,    2    );//D10
    scu_pinmux(    5    ,    7    ,    MD_PLN_FAST    ,    2    );//D11
    scu_pinmux(    6    ,    1    ,    MD_PLN_FAST    ,    1    );//DYCS1    
    scu_pinmux(    6    ,    3    ,    MD_PLN_FAST    ,    3    );//CS1
    scu_pinmux(    6    ,    4    ,    MD_PLN_FAST    ,    3    );//CAS
    scu_pinmux(    6    ,    5    ,    MD_PLN_FAST    ,    3    );//RAS
    scu_pinmux(    6    ,    6    ,    MD_PLN_FAST    ,    1    );//BLS1
    scu_pinmux(    6    ,    7    ,    MD_PLN_FAST    ,    1    );//A15
    scu_pinmux(    6    ,    8    ,    MD_PLN_FAST    ,    1    );//A14
    scu_pinmux(    6    ,    9    ,    MD_PLN_FAST    ,    3    );//DYCS0
    scu_pinmux(    6    ,    10    ,    MD_PLN_FAST    ,    3    );//DQMOUT1
    scu_pinmux(    6    ,    11    ,    MD_PLN_FAST    ,    3    );//CKEOUT0
    scu_pinmux(    6    ,    12    ,    MD_PLN_FAST    ,    3    );//DQMOUT0
    scu_pinmux(    10    ,    4    ,    MD_PLN_FAST    ,    3    );//A23
    scu_pinmux(    13    ,    0    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    2    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    3    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    4    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    5    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    6    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    7    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    8    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    9    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    10    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    12    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    13    ,    MD_PLN_FAST    ,    2    );//
    scu_pinmux(    13    ,    11    ,    MD_PLN_FAST    ,    2    );//CS3
    scu_pinmux(    13    ,    14    ,    MD_PLN_FAST    ,    2    );//DYCS2
    scu_pinmux(    13    ,    15    ,    MD_PLN_FAST    ,    2    );//A17
    scu_pinmux(    13    ,    16    ,    MD_PLN_FAST    ,    2    );//A16
    scu_pinmux(    14    ,    0    ,    MD_PLN_FAST    ,    3    );//A18
    scu_pinmux(    14    ,    1    ,    MD_PLN_FAST    ,    3    );//A19
    scu_pinmux(    14    ,    2    ,    MD_PLN_FAST    ,    3    );//A20
    scu_pinmux(    14    ,    3    ,    MD_PLN_FAST    ,    3    );//A21
    scu_pinmux(    14    ,    4    ,    MD_PLN_FAST    ,    3    );//A22
    scu_pinmux(    14    ,    5    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    6    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    7    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    8    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    9    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    10    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    11    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    12    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    13    ,    MD_PLN_FAST    ,    3    );

    /* Select EMC clock-out */
    LPC_SCU->SFSCLK_0 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_1 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_2 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_3 = MD_PLN_FAST;

    TIM_ConfigStruct.PrescaleOption = TIM_PRESCALE_USVAL;
    TIM_ConfigStruct.PrescaleValue    = 1;

    // Set configuration for Tim_config and Tim_MatchConfig
    TIM_Init(LPC_TIMER0, TIM_TIMER_MODE,&TIM_ConfigStruct);

    LPC_EMC->CONTROL     = 0x00000001;
    LPC_EMC->CONFIG      = 0x00000000;
    LPC_EMC->DYNAMICCONFIG0    = 0<<19 | 1<<12 | 1<<10 | 1<<7; /* 128Mb, 8Mx16, 4 banks, row=12, column=9 */

    pclk = CGU_GetPCLKFrequency(CGU_PERIPHERAL_M4CORE);

    _DBG("pclk = ");
    _DBD32(pclk);
    
    LPC_EMC->DYNAMICRASCAS0    = 0x00000303; /* 1 RAS, 3 CAS latency */
    LPC_EMC->DYNAMICREADCONFIG = 0x00000001; /* Command delayed strategy, using EMCCLKDELAY */

    LPC_EMC->DYNAMICRP         = NS2CLK(pclk, 20);
    LPC_EMC->DYNAMICRAS        = NS2CLK(pclk, 42);
    LPC_EMC->DYNAMICSREX       = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICAPR        = 0x00000005;
    LPC_EMC->DYNAMICDAL        = 0x00000005;
    LPC_EMC->DYNAMICWR         = 2;
    LPC_EMC->DYNAMICRC         = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICRFC        = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICXSR        = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICRRD        = NS2CLK(pclk, 14);
    LPC_EMC->DYNAMICMRD        = 0x00000002;

    TIM_Waitus(100);                           /* wait 100ms */
    LPC_EMC->DYNAMICCONTROL    = 0x00000183; /* Issue NOP command */

    TIM_Waitus(200);                           /* wait 200ms */
    LPC_EMC->DYNAMICCONTROL    = 0x00000103; /* Issue PALL command */
  

    LPC_EMC->DYNAMICREFRESH    = EMC_SDRAM_REFRESH(pclk,70); /* ( n * 16 ) -> 32 clock cycles */

    //for(i = 0; i < 0x80; i++);               /* wait 128 AHB clock cycles */
    TIM_Waitus(200);                           /* wait 200ms */

    tmpclk = (uint32_t)15625*(uint32_t)pclk/1000000000/16;
    LPC_EMC->DYNAMICREFRESH    = tmpclk; /* ( n * 16 ) -> 736 clock cycles -> 15.330uS at 48MHz <= 15.625uS ( 64ms / 4096 row ) */

    LPC_EMC->DYNAMICCONTROL    = 0x00000083; /* Issue MODE command */

    //Timing for 48/60/72MHZ Bus
    temp = *((volatile uint32_t *) 0x28023000);//(SDRAM_ADDR_BASE | (0x23<<12)) );//(3<<4| 3)<<11)); /* 4 burst, 3 CAS latency */
    temp = temp;
    LPC_EMC->DYNAMICCONTROL    = 0x00000000; /* Issue NORMAL command */

    //[re]enable buffers
    LPC_EMC->DYNAMICCONFIG0    |= 1<<19;

}

after init, i used this code

#define FRAMEBUFFER_ADDR        0x28000000

len = 64;

memcpy((uint8_t *)FRAMEBUFFER_ADDR,Buffer720,len);

This will successfully copy 64 bytes. Length above 64 is not working.

Also, if the code is like this, I can copy upto 256 Bytes.

len = 64;

    for( i=0;i<4;i++)
    {
        memcpy((uint8_t *)FRAMEBUFFER_ADDR+(i*64),Buffer720+(i*64),len);

        memcmp(FrameBuff,(uint8_t *)FRAMEBUFFER_ADDR+(i*64),len);

    }

ie, if reading the values after each 64 bytes, it can copy upto 256 Bytes.

What is wrong in this? Can anyone help me to solve this?

タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,837件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the AN11508, this application note describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

http://cache.nxp.com/documents/application_note/AN11508.pdf 

I hope this helps!!

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,837件の閲覧回数
ursaminor
Contributor II

You set DYNAMICRASCAS0=0x303, so the SDRAM mode word for a 16-bit bus is 0x33, not 0x23. (CAS=3, burst length=8).

You set DYNAMICCONFIG0=0x1480, which selects BRC addressing. In this case you must set the mode register by a dummy read from address 0x28000000+(0x33 << 10).

If you want high-performance mode (RBC addressing), set DYNAMICCONFIG0=0x0480, and use address 0x28000000+(0x33 << 12) for the mode register.

I assume you have hooked up the SDRAM bank selects to A13 and A14.

EDIT: just saw you have shown that in the connection list. However, is it true that you have connected A1...A12 to the SDRAM? This must be A0...A11!

0 件の賞賛
返信

3,837件の閲覧回数
tintuthomas
Contributor I

Hi ursaminor‌,


You set DYNAMICRASCAS0=0x303, so the SDRAM mode word for a 16-bit bus is 0x33, not 0x23. (CAS=3, burst length=8).

 

You set DYNAMICCONFIG0=0x1480, which selects BRC addressing. In this case you must set the mode register by a dummy read from address 0x28000000+(0x33 << 10).

If you want high-performance mode (RBC addressing), set DYNAMICCONFIG0=0x0480, and use address 0x28000000+(0x33 << 12) for the mode register.

 

I changed the code as u said. Still no change.

I assume you have hooked up the SDRAM bank selects to A13 and A14.

Yes BA0 to A13 and BA1 to A14.

EDIT: just saw you have shown that in the connection list. However, is it true that you have connected A1...A12 to the SDRAM? This must be A0...A11!

At first I connected A0 to A11. That was also not working . So after some reading , I found this post https://www.lpcware.com/content/forum/lpc43xx-interface-sdram.

In this on a comment bavarian says like this ,

"a 16-bit device normally starts with a connection of MCU_ADDR_1 to its A0 pin.
With a 16-bit device you don't use MCU_ADDR_0 at all, the byte addressing is done with LB and UB."

And I could see a connection picture in User manual UM10503 section 23.8.6 External static memory interface

16bitSDRAM.png

Here it shows connection from MCU as A[a_b:1] . Is it applicable to Dynamic memories?

Anyway both connections are not working...

0 件の賞賛
返信