SDRAM interfacing Problem with lpc4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM interfacing Problem with lpc4357

4,691 Views
tintuthomas
Contributor I

Hi all,

I am trying to interface SDRAM - AS4C8M16SA from Alliance, with LPC4357 (LQFP208 package). I'm not familiar with EMC or SDRAM. I got the RAM get initialized. But ,I cannot successfully write beyond 64 bytes into it. My connection details and initialization code are given below.


SDRAM Details

  •     Alliance AS4C8M16SA
  •     128M - 8M x 16 bit , 2M word x 16-bit x 4-bank
  •     CAS Latency: 2, or 3
         Burst Length: 1, 2, 4, 8, or full page
         Burst Type:  Sequential or Interleaved
  •      4096 refresh cycles/64ms

Connections

SDRAM                            LPC4357

DQ0 - DQ15            EMC_D0 - EMC_D15

A0 - A11                   EMC_A1 - EMC_A12

BA0                          EMC_A13

BA1                          EMC_A14

RAS                         EMC_RAS

CAS                         EMC_CAS

CS                           EMC_DYCS0

WE                          EMC_WE

NC/RFU                   NC

LDQM                      EMC_DQMOUT0

UDQM                      EMC_DQMOUT1

CLK                          EMC_CLK0

CKE                          EMC_CKEOUT0

Note: EMC_A6, EMC_A7, EMC_A8 and EMC_A0 pins are connected to some pull-up circuits to select the ISP method. The connection picture is attached.

Code

void SDRAM_Init () {
    uint32_t pclk, temp;
    uint32_t tmpclk;
    TIM_TIMERCFG_Type TIM_ConfigStruct;
    
    /* Set up EMC pin */
    scu_pinmux(    1    ,    0    ,    MD_PLN_FAST    ,    2    );    //A5
    scu_pinmux(    1    ,    1    ,    MD_PLN_FAST    ,    2    );    //A6
    scu_pinmux(    1    ,    2    ,    MD_PLN_FAST    ,    2    );    //A7
    scu_pinmux(    1    ,    3    ,    MD_PLN_FAST    ,    3    );    //OE
    scu_pinmux(    1    ,    4    ,    MD_PLN_FAST    ,    3    );    //BLS0
    scu_pinmux(    1    ,    5    ,    MD_PLN_FAST    ,    3    );    //CS0
    scu_pinmux(    1    ,    6    ,    MD_PLN_FAST    ,    3    );    //WE
    scu_pinmux(    1    ,    7    ,    MD_PLN_FAST    ,    3    );//D0
    scu_pinmux(    1    ,    8    ,    MD_PLN_FAST    ,    3    );//D1
    scu_pinmux(    1    ,    9    ,    MD_PLN_FAST    ,    3    );//D2
    scu_pinmux(    1    ,    10    ,    MD_PLN_FAST    ,    3    );//D3
    scu_pinmux(    1    ,    11    ,    MD_PLN_FAST    ,    3    );//D4
    scu_pinmux(    1    ,    12    ,    MD_PLN_FAST    ,    3    );//D5
    scu_pinmux(    1    ,    13    ,    MD_PLN_FAST    ,    3    );//D6
    scu_pinmux(    1    ,    14    ,    MD_PLN_FAST    ,    3    );//D7
    scu_pinmux(    2    ,    0    ,    MD_PLN_FAST    ,    2    );//A13
    scu_pinmux(    2    ,    1    ,    MD_PLN_FAST    ,    2    );//A12
    scu_pinmux(    2    ,    2    ,    MD_PLN_FAST    ,    2    );//A11
    scu_pinmux(    2    ,    6    ,    MD_PLN_FAST    ,    2    );//A10
    scu_pinmux(    2    ,    7    ,    MD_PLN_FAST    ,    3    );//A9
    scu_pinmux(    2    ,    8    ,    MD_PLN_FAST    ,    3    );//A8
    scu_pinmux(    2    ,    9    ,    MD_PLN_FAST    ,    0    );//A0// changed as GPIO
    scu_pinmux(    2    ,    10    ,    MD_PLN_FAST    ,    3    );//A1
    scu_pinmux(    2    ,    11    ,    MD_PLN_FAST    ,    3    );//A2
    scu_pinmux(    2    ,    12    ,    MD_PLN_FAST    ,    3    );//A3
    scu_pinmux(    2    ,    13    ,    MD_PLN_FAST    ,    3    );//A4
    scu_pinmux(    5    ,    0    ,    MD_PLN_FAST    ,    2    );//D12
    scu_pinmux(    5    ,    1    ,    MD_PLN_FAST    ,    2    );//D13
    scu_pinmux(    5    ,    2    ,    MD_PLN_FAST    ,    2    );//D14
    scu_pinmux(    5    ,    3    ,    MD_PLN_FAST    ,    2    );//D15
    scu_pinmux(    5    ,    4    ,    MD_PLN_FAST    ,    2    );//D8
    scu_pinmux(    5    ,    5    ,    MD_PLN_FAST    ,    2    );//D9
    scu_pinmux(    5    ,    6    ,    MD_PLN_FAST    ,    2    );//D10
    scu_pinmux(    5    ,    7    ,    MD_PLN_FAST    ,    2    );//D11
    scu_pinmux(    6    ,    1    ,    MD_PLN_FAST    ,    1    );//DYCS1    
    scu_pinmux(    6    ,    3    ,    MD_PLN_FAST    ,    3    );//CS1
    scu_pinmux(    6    ,    4    ,    MD_PLN_FAST    ,    3    );//CAS
    scu_pinmux(    6    ,    5    ,    MD_PLN_FAST    ,    3    );//RAS
    scu_pinmux(    6    ,    6    ,    MD_PLN_FAST    ,    1    );//BLS1
    scu_pinmux(    6    ,    7    ,    MD_PLN_FAST    ,    1    );//A15
    scu_pinmux(    6    ,    8    ,    MD_PLN_FAST    ,    1    );//A14
    scu_pinmux(    6    ,    9    ,    MD_PLN_FAST    ,    3    );//DYCS0
    scu_pinmux(    6    ,    10    ,    MD_PLN_FAST    ,    3    );//DQMOUT1
    scu_pinmux(    6    ,    11    ,    MD_PLN_FAST    ,    3    );//CKEOUT0
    scu_pinmux(    6    ,    12    ,    MD_PLN_FAST    ,    3    );//DQMOUT0
    scu_pinmux(    10    ,    4    ,    MD_PLN_FAST    ,    3    );//A23
    scu_pinmux(    13    ,    0    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    2    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    3    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    4    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    5    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    6    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    7    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    8    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    9    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    10    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    12    ,    MD_PLN_FAST    ,    2    );
    scu_pinmux(    13    ,    13    ,    MD_PLN_FAST    ,    2    );//
    scu_pinmux(    13    ,    11    ,    MD_PLN_FAST    ,    2    );//CS3
    scu_pinmux(    13    ,    14    ,    MD_PLN_FAST    ,    2    );//DYCS2
    scu_pinmux(    13    ,    15    ,    MD_PLN_FAST    ,    2    );//A17
    scu_pinmux(    13    ,    16    ,    MD_PLN_FAST    ,    2    );//A16
    scu_pinmux(    14    ,    0    ,    MD_PLN_FAST    ,    3    );//A18
    scu_pinmux(    14    ,    1    ,    MD_PLN_FAST    ,    3    );//A19
    scu_pinmux(    14    ,    2    ,    MD_PLN_FAST    ,    3    );//A20
    scu_pinmux(    14    ,    3    ,    MD_PLN_FAST    ,    3    );//A21
    scu_pinmux(    14    ,    4    ,    MD_PLN_FAST    ,    3    );//A22
    scu_pinmux(    14    ,    5    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    6    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    7    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    8    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    9    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    10    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    11    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    12    ,    MD_PLN_FAST    ,    3    );
    scu_pinmux(    14    ,    13    ,    MD_PLN_FAST    ,    3    );

    /* Select EMC clock-out */
    LPC_SCU->SFSCLK_0 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_1 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_2 = MD_PLN_FAST;
    LPC_SCU->SFSCLK_3 = MD_PLN_FAST;

    TIM_ConfigStruct.PrescaleOption = TIM_PRESCALE_USVAL;
    TIM_ConfigStruct.PrescaleValue    = 1;

    // Set configuration for Tim_config and Tim_MatchConfig
    TIM_Init(LPC_TIMER0, TIM_TIMER_MODE,&TIM_ConfigStruct);

    LPC_EMC->CONTROL     = 0x00000001;
    LPC_EMC->CONFIG      = 0x00000000;
    LPC_EMC->DYNAMICCONFIG0    = 0<<19 | 1<<12 | 1<<10 | 1<<7; /* 128Mb, 8Mx16, 4 banks, row=12, column=9 */

    pclk = CGU_GetPCLKFrequency(CGU_PERIPHERAL_M4CORE);

    _DBG("pclk = ");
    _DBD32(pclk);
    
    LPC_EMC->DYNAMICRASCAS0    = 0x00000303; /* 1 RAS, 3 CAS latency */
    LPC_EMC->DYNAMICREADCONFIG = 0x00000001; /* Command delayed strategy, using EMCCLKDELAY */

    LPC_EMC->DYNAMICRP         = NS2CLK(pclk, 20);
    LPC_EMC->DYNAMICRAS        = NS2CLK(pclk, 42);
    LPC_EMC->DYNAMICSREX       = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICAPR        = 0x00000005;
    LPC_EMC->DYNAMICDAL        = 0x00000005;
    LPC_EMC->DYNAMICWR         = 2;
    LPC_EMC->DYNAMICRC         = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICRFC        = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICXSR        = NS2CLK(pclk, 63);
    LPC_EMC->DYNAMICRRD        = NS2CLK(pclk, 14);
    LPC_EMC->DYNAMICMRD        = 0x00000002;

    TIM_Waitus(100);                           /* wait 100ms */
    LPC_EMC->DYNAMICCONTROL    = 0x00000183; /* Issue NOP command */

    TIM_Waitus(200);                           /* wait 200ms */
    LPC_EMC->DYNAMICCONTROL    = 0x00000103; /* Issue PALL command */
  

    LPC_EMC->DYNAMICREFRESH    = EMC_SDRAM_REFRESH(pclk,70); /* ( n * 16 ) -> 32 clock cycles */

    //for(i = 0; i < 0x80; i++);               /* wait 128 AHB clock cycles */
    TIM_Waitus(200);                           /* wait 200ms */

    tmpclk = (uint32_t)15625*(uint32_t)pclk/1000000000/16;
    LPC_EMC->DYNAMICREFRESH    = tmpclk; /* ( n * 16 ) -> 736 clock cycles -> 15.330uS at 48MHz <= 15.625uS ( 64ms / 4096 row ) */

    LPC_EMC->DYNAMICCONTROL    = 0x00000083; /* Issue MODE command */

    //Timing for 48/60/72MHZ Bus
    temp = *((volatile uint32_t *) 0x28023000);//(SDRAM_ADDR_BASE | (0x23<<12)) );//(3<<4| 3)<<11)); /* 4 burst, 3 CAS latency */
    temp = temp;
    LPC_EMC->DYNAMICCONTROL    = 0x00000000; /* Issue NORMAL command */

    //[re]enable buffers
    LPC_EMC->DYNAMICCONFIG0    |= 1<<19;

}

after init, i used this code

#define FRAMEBUFFER_ADDR        0x28000000

len = 64;

memcpy((uint8_t *)FRAMEBUFFER_ADDR,Buffer720,len);

This will successfully copy 64 bytes. Length above 64 is not working.

Also, if the code is like this, I can copy upto 256 Bytes.

len = 64;

    for( i=0;i<4;i++)
    {
        memcpy((uint8_t *)FRAMEBUFFER_ADDR+(i*64),Buffer720+(i*64),len);

        memcmp(FrameBuff,(uint8_t *)FRAMEBUFFER_ADDR+(i*64),len);

    }

ie, if reading the values after each 64 bytes, it can copy upto 256 Bytes.

What is wrong in this? Can anyone help me to solve this?

Tags (3)
0 Kudos
Reply
3 Replies

3,819 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the AN11508, this application note describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

http://cache.nxp.com/documents/application_note/AN11508.pdf 

I hope this helps!!

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,819 Views
ursaminor
Contributor II

You set DYNAMICRASCAS0=0x303, so the SDRAM mode word for a 16-bit bus is 0x33, not 0x23. (CAS=3, burst length=8).

You set DYNAMICCONFIG0=0x1480, which selects BRC addressing. In this case you must set the mode register by a dummy read from address 0x28000000+(0x33 << 10).

If you want high-performance mode (RBC addressing), set DYNAMICCONFIG0=0x0480, and use address 0x28000000+(0x33 << 12) for the mode register.

I assume you have hooked up the SDRAM bank selects to A13 and A14.

EDIT: just saw you have shown that in the connection list. However, is it true that you have connected A1...A12 to the SDRAM? This must be A0...A11!

0 Kudos
Reply

3,819 Views
tintuthomas
Contributor I

Hi ursaminor‌,


You set DYNAMICRASCAS0=0x303, so the SDRAM mode word for a 16-bit bus is 0x33, not 0x23. (CAS=3, burst length=8).

 

You set DYNAMICCONFIG0=0x1480, which selects BRC addressing. In this case you must set the mode register by a dummy read from address 0x28000000+(0x33 << 10).

If you want high-performance mode (RBC addressing), set DYNAMICCONFIG0=0x0480, and use address 0x28000000+(0x33 << 12) for the mode register.

 

I changed the code as u said. Still no change.

I assume you have hooked up the SDRAM bank selects to A13 and A14.

Yes BA0 to A13 and BA1 to A14.

EDIT: just saw you have shown that in the connection list. However, is it true that you have connected A1...A12 to the SDRAM? This must be A0...A11!

At first I connected A0 to A11. That was also not working . So after some reading , I found this post https://www.lpcware.com/content/forum/lpc43xx-interface-sdram.

In this on a comment bavarian says like this ,

"a 16-bit device normally starts with a connection of MCU_ADDR_1 to its A0 pin.
With a 16-bit device you don't use MCU_ADDR_0 at all, the byte addressing is done with LB and UB."

And I could see a connection picture in User manual UM10503 section 23.8.6 External static memory interface

16bitSDRAM.png

Here it shows connection from MCU as A[a_b:1] . Is it applicable to Dynamic memories?

Anyway both connections are not working...

0 Kudos
Reply