SDRAM configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM configuration

1,266件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tom-gds on Thu May 16 03:02:17 MST 2013

I'm designing a board using the LPC4357FET256 and want to use the maximum amount of SDRAM available per chip select (only the first CS will be populated initially but others may be later)


By far the cheapest solution is to use two RAM chips each in 64Mx16 configuration on each bus or a single chip in 64Mx32 configuration, however looking at the manual (page 484) it only gives an EMC address configuration option for using 4 chips in 64Mx8 configuration. This seems to be the only method that will allow me to use the maximum 2Gb per CS but not only works out more expensive than the other options but also takes up a lot more board space. Is it possible to set the address configuration to 64Mx8 and still only use two 64Mx16 chips or a single 64Mx32 chip?


I'm not sure how this would impact the number of rows and columns required but I would have thought it would be the same since the address space is identical, I'm simply splitting the 32 bit word into 1 or 2 instead of 4.


Thanks,


Tom

ラベル(1)
0 件の賞賛
返信
1 返信

1,232件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Fri May 24 10:09:45 MST 2013

Hello Tom,

you can achieve the maximum SDRAM size for example with this configuration:


- use two 16-bit memories in parallel, one gets connected to DQMOUT[1:0], the other one to DQMOUT[3:2], both on DYCS[0]


- we achieved this e.g. with MT48LC16M16 (256Mbit(16Mb x 4 x 4 bank)


There is an app note here:  http://www.lpcware.com/content/nxpfile/an10935-using-sdrddr-sdram-memories-lpc32xx


... which gives some good information about SDRAM. Its for another processor, but the SDRAM part is true for the LPC4300 as well.


A possible init sequence is shown below:


 


 


<p class="MsoPlainText">#if (USE_EXT_DYN_MEM_CS0)
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_SCU-&gt;EMCDELAYCLK = 0x00005555;
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>/* Set Address mapping for MT48LC16M16 cascaded as 32-bit memory: */
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>/* 256Mbit(16Mb x 4 x 4 banks), row len = 13, column len = 10<span style="mso-spacerun: yes;">     </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>/* bit[14] = 1<span style="mso-spacerun: yes;">    </span>bit]11:9] = 100<span style="mso-spacerun: yes;">   </span>bit[8:7] = 01<span style="mso-spacerun: yes;">                 </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONFIG0<span style="mso-spacerun: yes;">    </span>= (1 &lt;&lt; 14) |<span style="mso-spacerun: yes;">  </span>/* AM[14]<span style="mso-spacerun: yes;">   </span>= 1<span style="mso-spacerun: yes;">                   </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">                                                   </span>(0 &lt;&lt; 12) |<span style="mso-spacerun: yes;">  </span>/* AM[12]<span style="mso-spacerun: yes;">   </span>= 0<span style="mso-spacerun: yes;">                   </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">                                                   </span>(4 &lt;&lt;<span style="mso-spacerun: yes;">  </span>9) |<span style="mso-spacerun: yes;">  </span>/* AM[11:9] = 4<span style="mso-spacerun: yes;">                   </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">                                                   </span>(1 &lt;&lt;<span style="mso-spacerun: yes;">  </span>7) ;<span style="mso-spacerun: yes;">  </span>/* AM[8:7]<span style="mso-spacerun: yes;">  </span>= 1<span style="mso-spacerun: yes;">                   </span>*/
<p class="MsoPlainText"> <span style="mso-spacerun: yes;">  </span>LPC_EMC-&gt;DYNAMICRASCAS0<span style="mso-spacerun: yes;">    </span>= 0x00000303;<span style="mso-spacerun: yes;">  </span>/* Latency: RAS 3, CAS 3 CCLK cyc.*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICREADCONFIG = 0x00000001;<span style="mso-spacerun: yes;">  </span>/* Command delayed by 1/2 CCLK<span style="mso-spacerun: yes;">    </span>*
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICRP<span style="mso-spacerun: yes;">    </span>= 1;<span style="mso-spacerun: yes;">   </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICRAS <span style="mso-tab-count: 1;"> </span>= 3;
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICSREX <span style="mso-tab-count: 1;"> </span>= 6;<span style="mso-spacerun: yes;">   </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICAPR <span style="mso-tab-count: 1;"> </span>= 0;<span style="mso-spacerun: yes;">   </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICDAL <span style="mso-tab-count: 1;"> </span>= 5;<span style="mso-spacerun: yes;">   </span><span style="mso-tab-count: 1;">    </span>
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICWR <span style="mso-tab-count: 1;">   </span>= 1;
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICRC <span style="mso-tab-count: 1;">  </span>= 5;<span style="mso-spacerun: yes;">   </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICRFC <span style="mso-tab-count: 1;"> </span>= 5;<span style="mso-spacerun: yes;">    </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICXSR <span style="mso-tab-count: 1;"> </span>= 6;<span style="mso-spacerun: yes;">  </span>
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICRRD <span style="mso-tab-count: 1;"> </span>= 0;
<p class="MsoPlainText"><span style="mso-tab-count: 1;">   </span>LPC_EMC-&gt;DYNAMICMRD <span style="mso-tab-count: 1;"> </span>= 0;<span style="mso-spacerun: yes;">  </span>
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (10);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL<span style="mso-spacerun: yes;">    </span>= 0x00000183;<span style="mso-spacerun: yes;">  </span>/* Issue NOP command<span style="mso-spacerun: yes;">              </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (10);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL<span style="mso-spacerun: yes;">    </span>= 0x00000103;<span style="mso-spacerun: yes;">  </span>/* Issue PALL command<span style="mso-spacerun: yes;">             </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (1);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL<span style="mso-spacerun: yes;">    </span>= 0x00000183;<span style="mso-spacerun: yes;">  </span>/* Issue NOP command <span style="mso-spacerun: yes;">             </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (1);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICREFRESH<span style="mso-spacerun: yes;">    </span>= 2;<span style="mso-spacerun: yes;">   </span>//EMC_NANOSEC(<span style="mso-spacerun: yes;">  </span>200, SystemCoreClock, div) / 16 + 1;
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (10);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICREFRESH<span style="mso-spacerun: yes;">    </span>= 110; //EMC_NANOSEC(15625, SystemCoreClock, div) / 16 + 1;
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WaitUs (10);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL<span style="mso-spacerun: yes;">    </span>= 0x00000083;<span style="mso-spacerun: yes;">  </span>/* Issue MODE command<span style="mso-spacerun: yes;">             </span>*/
<p class="MsoPlainText"> 
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>/* Mode register: Burst Length: 4, Burst Type: Sequential, CAS Latency: 3<span style="mso-spacerun: yes;">   </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>WR_MODE(((3 &lt;&lt; 4) | 2) &lt;&lt; 12);
<p class="MsoPlainText">   <span style="mso-spacerun: yes;"></span>// Follow with at least 2 NOPS
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL <span style="mso-tab-count: 1;"> </span>|=<span style="mso-spacerun: yes;">  </span>EMC_INIT(EMC_NOP);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL <span style="mso-tab-count: 1;"> </span>|=<span style="mso-spacerun: yes;">  </span>EMC_INIT(EMC_NOP);
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONTROL<span style="mso-spacerun: yes;">  </span>= 0x00000003;<span style="mso-spacerun: yes;">  </span>/* Issue NORMAL command<span style="mso-spacerun: yes;">               </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;DYNAMICCONFIG0 |= (1 &lt;&lt; 19);<span style="mso-spacerun: yes;">   </span>/* Enable buffer<span style="mso-spacerun: yes;">                      </span>*/
<p class="MsoPlainText"><span style="mso-spacerun: yes;">   </span>LPC_EMC-&gt;STATICCONFIG0<span style="mso-spacerun: yes;">  </span>|= (1 &lt;&lt; 19) ;<span style="mso-spacerun: yes;">  </span>/* Enable buffer<span style="mso-spacerun: yes;">                      </span>*/
<p class="MsoPlainText">#endif

 


<pre class="MsoPlainText"><!--[if gte mso 9]><xml>
<w:LatentStyles DefLockedState="false" DefUnhideWhenUsed="true"
  DefSemiHidden="true" DefQFormat="false" DefPriority="99"
  LatentStyleCount="267">
  <w:LsdException Locked="false" Priority="0" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Normal"/>
  <w:LsdException Locked="false" Priority="9" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="heading 1"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 2"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 3"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 4"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 5"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 6"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 7"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 8"/>
  <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 9"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 1"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 2"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 3"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 4"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 5"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 6"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 7"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 8"/>
  <w:LsdException Locked="false" Priority="39" Name="toc 9"/>
  <w:LsdException Locked="false" Priority="35" QFormat="true" Name="caption"/>
  <w:LsdException Locked="false" Priority="10" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Title"/>
  <w:LsdException Locked="false" Priority="1" Name="Default Paragraph Font"/>
  <w:LsdException Locked="false" Priority="11" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Subtitle"/>
  <w:LsdException Locked="false" Priority="22" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Strong"/>
  <w:LsdException Locked="false" Priority="20" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Emphasis"/>
  <w:LsdException Locked="false" Priority="59" SemiHidden="false"
   UnhideWhenUsed="false" Name="Table Grid"/>
  <w:LsdException Locked="false" UnhideWhenUsed="false" Name="Placeholder Text"/>
  <w:LsdException Locked="false" Priority="1" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="No Spacing"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 1"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 1"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 1"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 1"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 1"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 1"/>
  <w:LsdException Locked="false" UnhideWhenUsed="false" Name="Revision"/>
  <w:LsdException Locked="false" Priority="34" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="List Paragraph"/>
  <w:LsdException Locked="false" Priority="29" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Quote"/>
  <w:LsdException Locked="false" Priority="30" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Intense Quote"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 1"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 1"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 1"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 1"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 1"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 1"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 1"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 1"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 2"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 2"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 2"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 2"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 2"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 2"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 2"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 2"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 2"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 2"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 2"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 2"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 2"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 2"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 3"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 3"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 3"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 3"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 3"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 3"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 3"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 3"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 3"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 3"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 3"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 3"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 3"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 3"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 4"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 4"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 4"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 4"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 4"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 4"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 4"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 4"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 4"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 4"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 4"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 4"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 4"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 4"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 5"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 5"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 5"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 5"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 5"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 5"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 5"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 5"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 5"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 5"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 5"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 5"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 5"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 5"/>
  <w:LsdException Locked="false" Priority="60" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Shading Accent 6"/>
  <w:LsdException Locked="false" Priority="61" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light List Accent 6"/>
  <w:LsdException Locked="false" Priority="62" SemiHidden="false"
   UnhideWhenUsed="false" Name="Light Grid Accent 6"/>
  <w:LsdException Locked="false" Priority="63" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 1 Accent 6"/>
  <w:LsdException Locked="false" Priority="64" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Shading 2 Accent 6"/>
  <w:LsdException Locked="false" Priority="65" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 1 Accent 6"/>
  <w:LsdException Locked="false" Priority="66" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium List 2 Accent 6"/>
  <w:LsdException Locked="false" Priority="67" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 1 Accent 6"/>
  <w:LsdException Locked="false" Priority="68" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 2 Accent 6"/>
  <w:LsdException Locked="false" Priority="69" SemiHidden="false"
   UnhideWhenUsed="false" Name="Medium Grid 3 Accent 6"/>
  <w:LsdException Locked="false" Priority="70" SemiHidden="false"
   UnhideWhenUsed="false" Name="Dark List Accent 6"/>
  <w:LsdException Locked="false" Priority="71" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Shading Accent 6"/>
  <w:LsdException Locked="false" Priority="72" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful List Accent 6"/>
  <w:LsdException Locked="false" Priority="73" SemiHidden="false"
   UnhideWhenUsed="false" Name="Colorful Grid Accent 6"/>
  <w:LsdException Locked="false" Priority="19" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Subtle Emphasis"/>
  <w:LsdException Locked="false" Priority="21" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Intense Emphasis"/>
  <w:LsdException Locked="false" Priority="31" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Subtle Reference"/>
  <w:LsdException Locked="false" Priority="32" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Intense Reference"/>
  <w:LsdException Locked="false" Priority="33" SemiHidden="false"
   UnhideWhenUsed="false" QFormat="true" Name="Book Title"/>
  <w:LsdException Locked="false" Priority="37" Name="Bibliography"/>
  <w:LsdException Locked="false" Priority="39" QFormat="true" Name="TOC Heading"/>
</w:LatentStyles>
</xml><![endif]--><!--[if gte mso 10]>
<style>
/* Style Definitions */
table.MsoNormalTable
{mso-style-name:"Table Normal";
mso-tstyle-rowband-size:0;
mso-tstyle-colband-size:0;
mso-style-noshow:yes;
mso-style-priority:99;
mso-style-qformat:yes;
mso-style-parent:"";
mso-padding-alt:0cm 5.4pt 0cm 5.4pt;
mso-para-margin:0cm;
mso-para-margin-bottom:.0001pt;
mso-pagination:widow-orphan;
font-size:11.0pt;
font-family:"Calibri","sans-serif";
mso-ascii-font-family:Calibri;
mso-ascii-theme-font:minor-latin;
mso-hansi-font-family:Calibri;
mso-hansi-theme-font:minor-latin;
mso-bidi-font-family:"Times New Roman";
mso-bidi-theme-font:minor-bidi;}
</style>
<![endif]-->
One further design note: Please use the CLK2 pin for the SDRAM clock, it has a slightly better timing characteristic than the CLK0 pin.
Then you need to configure the CLK23 signal on the CLK2 pin (= func 5). CLK3 pin must be configured to func 0 at the same time.

Best regards,
NXP Technical Support Team
0 件の賞賛
返信