SDCARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDCARD

2,261 Views
Reventaseldan
Contributor I

In MCUXpresso all the SDK examples are getting debugged but the SDCARD sdk as well as the program that was before executable is not debuggibg right now.what might be the problem?

error: connection closed by GDB server

0 Kudos
Reply
4 Replies

2,256 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number and SDK example you are using? what is the problem and error message?

BR

XiangJun Rong

0 Kudos
Reply

2,254 Views
Reventaseldan
Contributor I
Hi,
the part number LPC54608 and the example is SDCARD FATFS

all the other programs like can sdram are getting debugged but when I debug the SDCARD sdk I am getting "connection closed by GDB server" as error and not getting debugged.Can u tell me the problem and solution?
0 Kudos
Reply

2,242 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Maybe the SDcard has FAT file system, it has issue if you debug.

BR

XiangJun Rong

0 Kudos
Reply

2,230 Views
Reventaseldan
Contributor I

Yes it is FAT file system

 

What could be the solution?

 

0 Kudos
Reply