SDCARD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDCARD

2,187件の閲覧回数
Reventaseldan
Contributor I

In MCUXpresso all the SDK examples are getting debugged but the SDCARD sdk as well as the program that was before executable is not debuggibg right now.what might be the problem?

error: connection closed by GDB server

0 件の賞賛
返信
4 返答(返信)

2,182件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you tell us the part number and SDK example you are using? what is the problem and error message?

BR

XiangJun Rong

0 件の賞賛
返信

2,180件の閲覧回数
Reventaseldan
Contributor I
Hi,
the part number LPC54608 and the example is SDCARD FATFS

all the other programs like can sdram are getting debugged but when I debug the SDCARD sdk I am getting "connection closed by GDB server" as error and not getting debugged.Can u tell me the problem and solution?
0 件の賞賛
返信

2,168件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Maybe the SDcard has FAT file system, it has issue if you debug.

BR

XiangJun Rong

0 件の賞賛
返信

2,156件の閲覧回数
Reventaseldan
Contributor I

Yes it is FAT file system

 

What could be the solution?

 

0 件の賞賛
返信