SD card support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,892件の閲覧回数
jimschimpf
Contributor II

Is there a library for the M0 processors (eg LPC11xx) that runs an SD card and supports the FAT file system ?

0 件の賞賛
返信
1 解決策
2,708件の閲覧回数
jimschimpf
Contributor II

Thank you I am studying your code, there is enough code that I hope I will be able to muddle through the Chinese.

--jim schimpf

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,709件の閲覧回数
jimschimpf
Contributor II

Thank you I am studying your code, there is enough code that I hope I will be able to muddle through the Chinese.

--jim schimpf

0 件の賞賛
返信
2,708件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jim

If your problem is solved, please help us mark the correct answer to close this question, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,706件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jim Schimpf,

   I have a LPC1114 project which contains SD and FATFS,  the comment is all wrote in Chinese, but it doesn't matter, you can refer to the code directly.

Wish it helps you!

If you still have problem, please contact me!

0 件の賞賛
返信